2016-02-01 02:16 AM
Hi, i'm trying to use timer2 to generate two output shifted by 90 degree, like an encoder emulator. The idea is using the period of the timer2 to set the frequency, and set two output compare ch2,ch3 to set the output.
This is the code i'm using to set the timers:
static
int
numPackets;
static
int
currentPackets;
void
setQuadraticOutputConfig(
long
frequency,
long
_numPackets,
long
direction)
{
numPackets = (_numPackets*2)-1;
currentPackets = 0;
double
tmp = 0;
unsigned
long
period = (TIMER_FREQ/(frequency*2)-1);
unsigned
long
pulseA = period/4;
unsigned
long
pulseB = pulseA*3;
TIM_ClockConfigTypeDef sClockSourceConfig;
TIM_MasterConfigTypeDef sMasterConfig;
TIM_OC_InitTypeDef sConfigOC;
htim2.Instance = TIM2;
htim2.Init.Prescaler = 0;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = period;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
HAL_TIM_Base_DeInit(&htim2);
HAL_TIM_Base_Init(&htim2);
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig);
HAL_TIM_OC_Init(&htim2);
sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig);
sConfigOC.OCMode = TIM_OCMODE_TOGGLE;
if
(direction)
sConfigOC.Pulse = pulseA;
else
sConfigOC.Pulse = pulseB;
sConfigOC.OCPolarity = TIM_OCPOLARITY_LOW;
sConfigOC.OCFastMode = TIM_OCFAST_ENABLE;
HAL_TIM_OC_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_2);
if
(direction)
sConfigOC.Pulse = pulseB;
else
sConfigOC.Pulse = pulseA;
HAL_TIM_OC_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_3);
TIM2->CNT = 0;
//Force timer2 to 0
HAL_TIM_OC_Start_IT(&htim2, TIM_CHANNEL_2);
HAL_TIM_OC_Start_IT(&htim2, TIM_CHANNEL_3);
HAL_TIM_Base_Start_IT(&htim2);
}
And this the interrupt:
void
HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
if
(htim == &htim2){
if
(currentPackets == numPackets)
{
HAL_TIM_OC_Stop(&htim2, TIM_CHANNEL_2);
HAL_TIM_OC_Stop(&htim2, TIM_CHANNEL_3);
HAL_TIM_Base_Stop(&htim2);
}
currentPackets++;
}
}
Sometimes the first output is smaller then the others:
2016-02-01 03:41 AM
Please, don't reply by opening the reply link into a new window/tab, because the broken forum software creates a new sub-thread which contains un-openable contributions and also does not update this thread's timestamp/position in the main list.
Also, in this particular thread, please don't reply to the above two posts which are members of the sub-thread, reply to this post or the original one. JW2016-02-01 04:46 AM
ok
2016-02-01 10:02 PM
@stuk
If you need to use the TIM2 interrupt, set the URS flag in CR1 instead of the UDIS flag. Then you will get IRQ's on counter rollover/under, but you won't get an IRQ when you reset the counter with the UG flag.2016-02-02 01:13 AM
Hi arnold_w,
Check this discussion aboutmanaging “Timer interrupt �?:
.You be inspired there from my recommendations.
-Hannibal