Posted on February 01, 2016 at 11:16
Hi, i'm trying to use timer2 to generate two output shifted by 90 degree, like an encoder emulator. The idea is using the period of the timer2 to set the frequency, and set two output compare ch2,ch3 to set t...
Posted on June 17, 2015 at 14:36Every time i move the scroolbar up or down, or left/right to resize the window, my project is closed, and i return to the startup page of the CubeMx! #bug #cubemx
Posted on June 17, 2015 at 11:19Hi, i've CubeMx 4.8.0 and i want update the firmware of the STM32F4 board with the new FW_F4_V1.6.0. When i open a project that used fw 1.5.0 i can't understand how can i update to the new 1.6.0 firmware, in the setti...
Posted on July 06, 2015 at 09:01I've similar problem, i solved becouse i've an old .ioc file (for old i mean a backup version before upgrade to 4.8.0). This works perfect.
Posted on June 17, 2015 at 14:26The same for me, its incredible released a new version if you can use it! I think CubeMx is a little joke tool, not a professional tool.
Posted on June 17, 2015 at 13:42 Hi, thanks for reply. Can you post me the link to the thread? I can't find it! Thanks [EDIT] Ok, after some research i found the https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/flat.aspx?Ro...