QSPI: Write/Read strings from QSPI memory
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-06 5:23 AM
Hello,
I implemented some functions to read and write the QSPI memory by using functions HAL_QSPI_Transmit() and HAL_QSPI_Receive() provided by the libraries.
Everything works fine. I just wonder how I can write and read strings using these functions.
I want to write:
char myString[100][50];
but the above functions have a uint8_t as an input!
Is there any way to do so, other than passing a single character at a time?
Thanks,
#read #strings #write #qspiSolved! Go to Solution.
- Labels:
-
QSPI
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-06 10:21 AM
Use a cast?
char myString[50];
BSP_QSPI_Write((void *)myString, Address, sizeof(myString));
BSP_QSPI_Write((uint8_t *)&myString[0], Address, sizeof(myString));
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-06 7:56 AM
>>Is there any way to do so, other than passing a single character at a time?
Clearly there would be a means to achieving it.
STM32Cube_FW_F7_V1.11.0\Drivers\BSP\STM32F769I-Discovery\stm32f769i_discovery_qspi.c
BSP_QSPI_Write(Buffer, Address, Size)
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-06 10:16 AM
Thanks!
But how can I put my string (let's say char myString[50]) inside the Buffer in
BSP_QSPI_Write()?
This function only accepts uint8_t as a buffer and I have a chars!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-06 10:21 AM
Use a cast?
char myString[50];
BSP_QSPI_Write((void *)myString, Address, sizeof(myString));
BSP_QSPI_Write((uint8_t *)&myString[0], Address, sizeof(myString));
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-06 10:28 AM
Thank you very much! I was casting in a wrong way..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-06 10:49 AM
>>Thank you very much! I was casting in a wrong way..
C can be like that, and the cast frequently stops the compiler complaining when it would be helpful that it did.
char myString[100][50];
BSP_QSPI_Write((void *)&myString[0][0], Address, sizeof(myString)); // Base address of my array - writing to QSPI FLASH as a binary blob
Several ways to do this, the form like this might be clearer to a subsequent reader of the code, or future self, that you really want the address of the base elements of the array as the starting point.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-08 7:45 AM
I have an additional question that comes to mind.
Instead of writing and reading the QSPI memory, can I use a variable to point to one of its block addresses?
For example, I want to point to the QSPI memory with a variable like this:
char myVariable[50]
I need an alternative to Write and Read because I need to write a lot and it takes to much time...
Thanks!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-08 10:27 AM
I don't believe you can write-in-place
Reading
char *myVariable = (char *)0x90001234;
You could do similar things using the linker script, or scatter file, to create a NOINIT region where you direct QSPI structures into.
Up vote any posts that you find helpful, it shows what's working..