PWM Input capture and PWM output with same timer
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-03-27 8:06 AM
Posted on March 27, 2015 at 16:06
Hi,
I'm working with an STM32F103RB.I try to do a PWM input capture (frequency and duty) and also PWM output with the same TIMER.It seems there is a problem.My pwm output restarts when a rising edge occurs on thepwminput.For the PWM Input capture, i'm using TIM3 channel 1 (and channel2 for duty cycle) and for PWMoutput, i'm using TIM3 channel 3.If I activate only the PWM Input, it works.And also, if I activate only the PWMOutput, it works.Is there a limitation or maybe I forget to disable a reset ?Thanks #stm32f103 #pwm #timer
Labels:
- Labels:
-
STM32F1 Series
-
TIM
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-03-27 8:12 AM
Posted on March 27, 2015 at 16:12
PWM Input resets the timer, that's how it works. The TIM only has a single counting element.
I don't see using the same timer to do measurement and PWM output, the periodicity of the timer is going to be rather limiting. If I really had to do this for myself, I'd using Input Capture, with a maximal period, using two channels to time stamp opposite edges, and I'd use Toggle Mode to control the output signal.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..