Skip to main content
Associate III
March 26, 2015
Question

LSE and HSE on MCO1

  • March 26, 2015
  • 4 replies
  • 987 views
Posted on March 26, 2015 at 09:56

I use STM32F4

I set MCO1 to PLL Clock and set output prescaler to 5 and I have 6MHz on my MCO1. There is no problem in it, But when I enable LSE with HSE together, I have no signal on MCO1 pin. Code:

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 25;
RCC_OscInitStruct.PLL.PLLN = 336;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 7;
HAL_RCC_OscConfig(&RCC_OscInitStruct);
HAL_RCC_MCOConfig(RCC_MCO1,RCC_MCO1SOURCE_PLLCLK,RCC_MCODIV_5);

What is the problem? Thanks...
    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    March 26, 2015
    Posted on March 26, 2015 at 13:38

    Does some other unshown code configure the other GPIOs and clocks to allow this to work?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Associate III
    March 26, 2015
    Posted on March 26, 2015 at 14:59

    Yes. GPIO configured with this code :

    __GPIOA_CLK_ENABLE();
    GPIO_InitStruct.Pin = GPIO_PIN_8;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_PULLDOWN;
    GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
    GPIO_InitStruct.Alternate = GPIO_AF0_MCO;
    HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

    When I change this line:

    RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSE;

    to

    RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;

    MCO1 clock is good and with LSE, I have no clock on MCO1 pin.
    waclawek.jan
    Super User
    March 26, 2015
    Posted on March 26, 2015 at 22:35

    Try to blink a LED in the main loop, first with the setting where you do have the output clock, then with the other setting.

    Does it blink in both cases?

    JW

    Associate III
    March 27, 2015
    Posted on March 27, 2015 at 13:33

    Yes.

    I have LED blinking every 500mS in both cases(cmsis_os delay) 

    and I have 1KHz signal of TIM3 too.

    -----------------

    In my new tests I have MCO1 clock in both cases!

    (No board changes and no software changes!)

    I am continuing my work and if this state happened again I will write state to this thread.

    Thanks.