cancel
Showing results for 
Search instead for 
Did you mean: 

PUPDR in GPIOD - default values are wrong

Tobe
Senior III

In the manual it states, that reset value is 0x000.., and that 0xFFFF... is reserved. But when debugging, i see, that it is 0xFF... . When now assigning a new value to it via HAL_GPIO_Init(), the register does not take the new values.

Hold on!

I just found the solution while writing this post:

Copied the code from another project, but forgot the part where the clock of that Port was activated!

1 ACCEPTED SOLUTION

Accepted Solutions
Tobe
Senior III

Couldnt mark my first entry as solution, so i write this reply ;)

View solution in original post

1 REPLY 1
Tobe
Senior III

Couldnt mark my first entry as solution, so i write this reply ;)