2025-01-27 04:37 AM
Hi,
I am using PSSI on STM32H7R3 to transmit data with DE output signal and RDY input signal (flow control). Incoming clock frequency is 60MHz. Data buffer is located in AHBSRAM1 and have size 4096 bytes. GPDMA feeds PSSI buffer by 32bit access (four bytes at once). Application while loop waits until DMA transfer complete and then restarts transfer again. Most of the time everything works OK, PSSI correctly reacts on RDY signal by "stopping" transmission (repeating data until RDY asserted), DE signal also works correctly except for one moment. When RDY (PSSI input) and DE (PSSI outout) are deasserted at the same time (clock), then PSSI makes "mistake" and retransmit one byte of data two times.
Data in SRAM buffer are OK (checked by debugger)
PSSI Configuration:
DERDYCFG = 0b11 (both DE + RDY signals used)
DMAEN = 1
OUTEN = 1
On following scope traces can be seen, that PSSI transmites "1" before RDY blocks data flow. When reciever is ready to accept data, asserts RDY and PSSI transmitt "1" again. Data consis of alternating 0 and 1, therefore PSSI should never transmit two same data consecutive.First transmittion after RDY assert
Lastr transmittion before RDY deassert
overall view
this event happens when program "reload" DMA (tracked by signal on PB8)
while (1)
{
while(!(LL_DMA_IsActiveFlag_TC(GPDMA1, LL_DMA_CHANNEL_0))){} // wait until DMA transfer complete
LL_GPIO_SetOutputPin(GPIOB, LL_GPIO_PIN_8); // indicate moment when DMA is reloaded
cnt++;
if(cnt >= 16){
cnt = 0;
}
LL_DMA_ClearFlag_TC(GPDMA1, LL_DMA_CHANNEL_0);
LL_DMA_SetBlkDataLength(GPDMA1, LL_DMA_CHANNEL_0,BLOCK_SIZE);
LL_DMA_SetSrcAddress(GPDMA1, LL_DMA_CHANNEL_0, DMA_SRC_ADDRESS);
LL_DMA_EnableChannel(GPDMA1, LL_DMA_CHANNEL_0);
LL_GPIO_ResetOutputPin(GPIOB, LL_GPIO_PIN_8); // indicate moment when DMA is reloaded
}
But when i add some delay into "DMA reload" routine, problem dissapears. Following scope trace show that situation:with delay, it is ok
but then another error appears somewhere else in the data instead. For now I am not able to locate them exactly to rule out that it is a problem in the receiver. Even so, the problem described above is enough to make the transmission unreliable.
Does anyone have any idea what to do with it?
Thanks,
Michal Dudka
2025-01-27 05:09 AM - edited 2025-01-27 05:24 AM
while (1){
if(PSSI->SR & PSSI_SR_RTT4B){
PSSI->DR = arr[idxx];
idxx++;
if(idxx >= BLOCK_SIZE){
LL_GPIO_SetOutputPin(GPIOB, LL_GPIO_PIN_8);
delay(1000);
idxx = 0;
cnt++;
if(cnt >= 16){
cnt = 0;
}
LL_GPIO_ResetOutputPin(GPIOB, LL_GPIO_PIN_8);
}
}
}
}