cancel
Showing results for 
Search instead for 
Did you mean: 

PROGRaming use of 2do usb in nucleo.h7

yogui_ricardo
Associate II

I want to use the second USB of my nucleo-h753zi board, in a program that checks and graphs the movements and clicks of the mouse that enters through the USB port, but I only see the stlink, there is the init = MX_USB_DEVICE_Init (void);  I used the power in "ext" and in "chgr" but without result.  What am I missing or what am I doing wrong? Thanks

 

yogui_ricardo_0-1730055814190.png

 

3 REPLIES 3
gbm
Principal

Middleware - USB device - select a proper class (CDC?) and write some code to handle the transfers.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
yogui_ricardo
Associate II

yes;That is contemplated:

void SendMessageToPC(char* message) {

CDC_Transmit_FS((uint8_t*)message, strlen(message));

}

void SendMovementData(int x, int y, uint8_t buttons) {

char buffer[50]; // Buffer para el mensaje

// Formatear el mensaje

sprintf(buffer, "Mov: X=%d, Y=%d, Buttons=%d\r\n", x, y, buttons);

// Enviar el mensaje al PC

CDC_Transmit_FS((uint8_t*)buffer, strlen(buffer));

}

void ProcessMovement() {

HID_ReportTypeDef report = {0, 0, 0}; // Inicializa el reporte

report.buttons = 1; // Emular clic en el botón 1

report.x = 5; // Desplazamiento en X

report.y = 0; // Desplazamiento en Y

USBD_HID_SendReport(&hUsbDeviceFS, (uint8_t*)&report, sizeof(report));

// Envía la información de movimiento por USB Serial

SendMovementData(report.x, report.y, report.buttons);

HAL_Delay(10); // Pausa para evitar sobrecarga de reportes

}

FBL
ST Employee

Hi @yogui_ricardo 

You need HID class instead of CDC to interface a mouse. Here is a working example to start with on eval board  STM32CubeH7/Projects/STM32H743I-EVAL/Applications/USB_Device/HID_Standalone at master · STMicroelectronics/STM32CubeH7 · GitHub You need to refer to schematics as well.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.