cancel
Showing results for 
Search instead for 
Did you mean: 

Program Upload method in nucleo stm32f103

yugi
Associate

Hello Everyone 
I am try to upload my code through stm32f103 necleo debuger or programmer but  have facing one issue for no st link found error 
I have attached the pic please give the solution .

4 REPLIES 4
AScha.3
Chief

Hi,

Was the nucleo/st-link working before ?

With same USB cable ?

If remove your external wires, then working?

If you feel a post has answered your question, please click "Accept as Solution".
Andrew Neil
Evangelist III

@yugi wrote:

 no st link found error 
I have attached the pic please give the solution .


Is the ST-Link being detected by the host computer?

eg, does the Virtual COM Port appear in the Device Manager?

AndrewNeil_0-1706630498139.png

If the host computer isn't detecting the ST-Link, then there's no way that any other app (eg, debugger or programmer) is going to be able to use it.

i'm check the stlink  in device manager is showing the stlink

 

Show a screenshot of the message(s) you receive

BTW: you can just paste an image into the post (as I did above) - no need to attach.