2024-08-14 5:33 AM - last edited on 2024-10-30 2:36 AM by mƎALLEm
Hi,
I have ported the Open Bootloader to the STM32G431 and has flashed it and is able to communicate with it over FD-CAN. Is there any program out there that I can use to flash programs using the bootloader over FD-CAN? maybe the CLI version of the STM32Cube programmer work? In that case is there a version for Linux on Arm of it (could only find amd64 version)?