cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743 Flash erase erases the wrong bank

Joni
Associate

Hi,

I am building a program that can flash new firmware onto a STM32H743ZIT6 via CAN. It does so by utilizing the dual bank feature and ping-ponging between bank 1 and bank 2. It receives the firmware via CAN and buffers it. Before writing it to the inactive bank it first erases said bank.

When running form bank 1 this works just fine and it is able to reboot to the newly flashed bank. When going from bank 2 back to bank 1 however, it encounters an issue. It crashes in the erase step and will not restart.

After I manually disable the SWAP_BANK bit using STM32CubeProgrammer it runs again on bank 1 without flashing again. This (I think) tells me it is deleting bank 2 while also running on it.

Attached you find the function in question, do you have any idea where i went wrong?

 

void foc_erase_inactive_bank() {
  // Determine inactive bank from SWAP_BANK bit
  uint8_t inactive_bank = (FLASH->OPTCR & FLASH_OPTCR_SWAP_BANK) ? 1 : 2;
  uint32_t bank_to_erase = (inactive_bank == 1) ? FLASH_BANK_1 : FLASH_BANK_2;

  LOG_INFO("FOC [ERASE] Starting mass erase of bank %u", inactive_bank);

  // unlock flash
  if (HAL_FLASH_Unlock() != HAL_OK) {
    LOG_ERROR("FOC [ERASE] HAL_FLASH_Unlock failed");
    foc.state = FOC_STATE_ERROR;
    return;
  }
  // Disable instruction cache prior to flash operation
  SCB_DisableICache();

  // Configure and execute mass erase
  FLASH_EraseInitTypeDef erase_init = {
      .TypeErase = FLASH_TYPEERASE_MASSERASE,
      .Banks = bank_to_erase,
      .VoltageRange = FLASH_VOLTAGE_RANGE_3,
  };

  uint32_t erase_error = 0U;
  HAL_StatusTypeDef erase_result = HAL_FLASHEx_Erase(&erase_init, &erase_error);

  // Re-enable cache and lock flash
  SCB_EnableICache();
  HAL_FLASH_Lock();

  // handle error
  if (erase_result != HAL_OK) {
    uint32_t hal_error = HAL_FLASH_GetError();
    LOG_ERROR(
        "FOC [ERASE] Mass erase failed with status %lu, HAL error: 0x%08X",
        (unsigned long)erase_result, hal_error);
    foc.state = FOC_STATE_ERROR;
    return;
  }

  LOG_INFO("FOC [ERASE] Successfully erased bank %u", inactive_bank);
}

 

3 REPLIES 3
Pavel A.
Super User

Is this STM32H743ZIT6  ?

Yes, absolutely, i mistyped. It's the STM32H743ZIT6. Thanks!

Saket_Om
ST Employee

Hello @Joni 

Please refer to the application note and the article below: 

STM32 in-application programming (IAP) using the USART - Application note

How to configure swap bank on STM32H7 part 1 - STMicroelectronics Community

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om