2021-08-27 1:22 PM
This is just a test. Has anybody else been unable to submit questions? I keep getting a red error message.
Solved! Go to Solution.
2021-08-27 2:05 PM
You're missing something, but it's not obvious. The down arrow on the top-right of the post lets you edit topics.
2021-08-27 1:25 PM
Lol, naturally the test question worked perfectly. Of course, my actual question is still failing with the error:
2021-08-27 1:55 PM
After a little more tinkering, it looks like the error is caused by selecting any topic for the post. The post works if no topics are entered. Weird bug.
2021-08-27 1:59 PM
You can edit topics after you submit the post as a workaround.
2021-08-27 2:02 PM
That's a good idea, but I don't see the topic field when I edit a post after submitting it. Am I just missing something obvious?
2021-08-27 2:05 PM
You're missing something, but it's not obvious. The down arrow on the top-right of the post lets you edit topics.
2021-08-27 2:09 PM
Thanks, that worked great. I stupidly assumed it would be under the regular Edit command and didn't notice the separate Edit Topics option. Excellent UI design, as always...
2021-08-27 7:30 PM
The other point of note is that your can't make up topics, only select existing ones