2017-03-07 11:44 AM
hello
i am working with STM32_MAT-TARGET in external mode i can generat project
help please
#stm32-mat-target #simulink #external #stm32-mat/target-matlabSolved! Go to Solution.
2017-03-12 06:03 AM
https://community.st.com/0D50X00009XkYEASA3
Mandatory Software :
matlab 2016 b
Keil version V 5.23
STM32CubMX 4.20
in the external mode : make sure thatHeapSize must behigher as possible.
make sure that the configuration of UART(Rx,Tx) in your stm32 it is connected to the USB (VCP_TX ,VCP_RX)
2017-03-08 12:46 AM
Hi abdou si,
Could you please precise theSTM32-MAT/TARGET and Keil version are you using ?
I suggest you to debug,identify what is the problem that you see and when it occurs orwhere the code hangs/stop.
I recommend you to follow the instructions in the attached document
'STM32 MAT-TARGET HandsOn'it may help you on your project.
Imen
________________ Attachments : STM32_MAT-TARGET_HandsOn_v1_0.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hypn&d=%2Fa%2F0X0000000bD0%2FBR9ZtSfu_Um8n1rd3cF4OzI8ZT4y4Ju1arNoCyuutLs&asPdf=false2017-03-08 04:37 AM
this for may application i am using GPIO in stm32f303k8
________________ Attachments : external.ioc.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hypd&d=%2Fa%2F0X0000000bCy%2FFbAg5KKa2SpZ_vY.DkU9dlj7jGBLDxp1zLK11gYm.2k&asPdf=false2017-03-08 04:59 AM
thanks Imen
i am working with KEIL V5 and
STM32-MAT/TARGET 4.4.1 in matlab 2016b i am alos working with STM32_MAT-TARGET_HandsOn
i took this exemple
i build it in external Mode i get this
2017-03-08 05:15 AM
Hi,
Could you please share your .ioc file as well the log files that can be found in your user directory under the .stm32cubemx folder.
Thanks
Imen
2017-03-08 05:21 AM
Hi,
I will share your issue internally to our CubeMx team for further investigation and come back to you as soon as possible.
Imen
2017-03-08 05:36 AM
whene i start the building i get this ioc file
________________ Attachments : external_extMode.ioc.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HypY&d=%2Fa%2F0X0000000bCw%2FRKjMBZOD.HniHU5mNc31lttiSsXYzhWW5VyHGzBuDvM&asPdf=false2017-03-08 06:43 AM
Which version of Keil are you using ? Try to update Keil tools (last version V5.23) if you are using an old version.
2017-03-08 09:45 AM
i am already using the 5.23 V
i wanna try with older version of STM32_MAT-TARGET for matlab 2015 b but i cant download can you help ?
2017-03-08 12:22 PM
How i can download STM32-MAT/TARGET 4.4.0