cancel
Showing results for 
Search instead for 
Did you mean: 

problem with STM32_MAT-TARGET in external mode

abdou si
Associate III
Posted on March 07, 2017 at 20:44

hello 

i am working with STM32_MAT-TARGET in external mode  i can generat project 

0690X00000603ijQAA.jpg

help please 

#stm32-mat-target #simulink #external #stm32-mat/target-matlab
15 REPLIES 15
Imen.D
ST Employee
Posted on March 09, 2017 at 10:30

Hi

You can find attached the previous versionSTM32-Mat/TARGET V4.4.0 as you asked.

But, I recommendto you using the latest version of STM32-MAT/TARGETwhich contains enhancement asST maintains its supportonly for the last version of

STM32Mat/TARGET

available on the ST web.

Imen

________________

Attachments :

STM32MatTarget_4.4.0_setup.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HynU&d=%2Fa%2F0X0000000bCt%2Fm3YTaBi3ugz8uz4QSxa6BhBCZELVeStlZISxXk9Zy7w&asPdf=false
When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Imen.D
ST Employee
Posted on March 09, 2017 at 16:03

I have copied your .ioc file in new folder and the project is successfully generated.

So, I think that the problem is related to your configuration setting with Keil.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
abdou si
Associate III
Posted on March 09, 2017 at 18:36

i can generated a project with .ioc but the problem when i use simulink externel mode i cant generat project you can see the PDF

https://community.st.com/servlet/JiveServlet/download/150568-1-7850/STM32_MAT-TARGET_HandsOn_v1_0.pdf

page 90

Posted on March 10, 2017 at 17:07

we aren't able to reproduce this error !

Please check that you are correctly configure Simulink Model Setting to use the correct parameters and the last version of CubeMx V4.20 (as mentioned in the attached document, in 'Simulink Model Setting' section)

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
abdou si
Associate III
Posted on March 12, 2017 at 11:13

thanks it is work

abdou si
Associate III
Posted on March 12, 2017 at 14:03

https://community.st.com/0D50X00009XkYEASA3

Mandatory Software :

matlab 2016 b

Keil version V 5.23

STM32CubMX 4.20

in the external mode : make sure thatHeapSize must behigher as possible.

make sure that the configuration of UART(Rx,Tx) in your stm32 it is connected to the USB (VCP_TX ,VCP_RX)