2015-02-10 12:46 AM
Hi to all, i use CubeMX and Keil 5.12 with Stm Nucleo, STM32L152RE, all work well.
Yesterday I upgrade the CubeMX to 4.6 version, later this upgrade i have this error: --- The Project references devices, files or libraries that are not installed Download and Install Third Party Device Support for ''STMicroelectronics :STM32L125RE'' (Device not included in Legancy Device Satabases)--- i upgrade Keil to the 5.13 version, in Pack Install i uninstall and later install the packeg for StM32L152 but don't work. if I open blink example all work well, if i use other easy example all work well, but if i use the code of CubeMx i have this message error. can you help me? best regards Antonio2015-07-01 2:40 AM