cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX 4.6 i2c settings messed up

mail239955_stm1
Associate
Posted on February 08, 2015 at 20:28

Tested on STM32F030C8x chip - when configuring i2c via CubeMX available options for ''Clock No Stretch Mode'' are ''Clock Stretch Enabled'' mapped to I2C_NOSTRETCH_ENABLED (and via macros to I2C_CR1_NOSTRETCH) which means that clock stretching is disabled, and ''Clock Stretch Disabled'' mapped to I2C_NOSTRETCH_DISABLED (which means that clock stretching is enabled).

Enabled/Disabled mappings must be reversed

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
stm32cube-t
ST Employee
Posted on July 01, 2015 at 11:43

Has been as part of MX 4.7.