cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with MX-generated code when BSP and ThreadX both enabled for Nucleo board

nicgreenway
Associate II

I have a project on a H563ZI Nucleo board, and noticed an issue when I enable both the Board Support Package (BSP) options and ThreadX.

The MX-generated code in main.c places the BSP initialisation after the call to MX_ThreadX_Init()  - see snippet below.  This means the BSP code is unreachable and the components are not initialised.

The workaround is simple (copy the BSP code into the USER CODE 2 section), but it should probably be looked at.

 

Snippet of automatically MX-generated code from main.c:

 

/* USER CODE END 2 */

 

MX_ThreadX_Init();

 

/* Initialize leds */

BSP_LED_Init(LED_GREEN);

BSP_LED_Init(LED_YELLOW);

BSP_LED_Init(LED_RED);

 

/* Initialize USER push-button, will be used to trigger an interrupt each time it's pressed.*/

BSP_PB_Init(BUTTON_USER, BUTTON_MODE_EXTI);

 

/* Initialize COM1 port (115200, 8 bits (7-bit data + 1 stop bit), no parity */

BspCOMInit.BaudRate = 115200;

BspCOMInit.WordLength = COM_WORDLENGTH_8B;

BspCOMInit.StopBits = COM_STOPBITS_1;

BspCOMInit.Parity = COM_PARITY_NONE;

BspCOMInit.HwFlowCtl = COM_HWCONTROL_NONE;

if (BSP_COM_Init(COM1, &BspCOMInit) != BSP_ERROR_NONE)

{

Error_Handler();

}

 

/* We should never get here as control is now taken by the scheduler */

 

/* Infinite loop */

/* USER CODE BEGIN WHILE */

1 REPLY 1
Souhaib MAZHOUD
ST Employee

Hello @nicgreenway 

Thank you for bringing this issue to our attention, I will check it internally and get back to you as soon as possible.

Thx

Souhaib