cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with Keil uVision 4: ''Failure loading STLinkUSBDriver.dll''

wolfram
Associate II
Posted on April 05, 2011 at 11:30

Hello,

when i try using the STM32 Discovery board (STM32F100)

with Keil uVision (V4.20.03.0, Target DLL: STLink\ST-LINKIII-KEIL.dll V1.5.6), when i try to debug or flash there always pops up this error:

''Failure loading STLinkUSBDriver.dll''.

This Dll exists in the path C:\Keil\ARM\STLink\,

but it just does not want to work.

Any help is appreciated.

Wolfram

12 REPLIES 12
lastsamurai
Associate III
Posted on May 17, 2011 at 02:04

HI Steahler,

Thanks for the smart solution.. Although it is a dirty one, working like a charm!

Cheers,

Sam

wolfram
Associate II
Posted on May 26, 2011 at 17:03

Hi

Ibtissem

,

the

ST-LINK V2 driver did the trick, thanks!

Wolfram

juozas
Associate III
Posted on September 10, 2011 at 16:45

My solution of problem:

Uninstall from Windows STLINK V2 soft, bacause this new STM32 ST-LINK Utility did not connects to my VLDISCOVERY. I'am happy did not delete older file um0892.zip (downloaded before 2011 March 18). After installing this older ST-LINK software I was able to connect to my VLDISCOVERY. To be happy with Keil environment : rename C:\Keil\ARM\STLink\STLinkUSBDriver.dll to ''..too_new...'' and copy older

STLinkUSBDriver

.dll (2008.09.24) to this directory from C:\Program Files\STMicroelectronics\STM32 ST-LINK Utility_old\ST-LINK Utility. You must be Windows Administrator group member to use ST-Link with Keil. This will not depend on language settings.

Regards,

Juozas Kimtys