User Activity

Hi, I configured FDCAN1 in classic format and was able to send CAN messages to a recipient. However, if I want to try the same with FDCAN2 it does not work and the TX FIFO gets full and goes to the error handler. However, If I change FDCAN_Config to ...
Posted on May 04, 2011 at 03:19HI, I have a problem with STM32VL discovery board.  When I try to connect to the board via SWD through ST-Link utility, I get the message that target is not connected!  But I can connect to the board through ST-Link me...