2015-12-15 1:05 AM
Hello, i am new to 32Bit world
i am using Atollic Lite the update version. my IC was STM32F103C8 and STM32F10x Standard Peripherals Library Drivers update History V3.6.1. I need to use printf to print thing to USART.I saw some thread that need to attach sys_call.c and tiny_printf.c? Is that true?
i follow some thread that use the following code:
nt _write(int file, char *ptr, int len)
{ /* Implement your write code here, this is used by puts and printf for example */ int i=0; for(i=0 ; i<len ; i++) USARTSendChar((*ptr++)); //<–this is my usart code return len; } however it doesnot work.i use normal USART to dump ascii to hyperterminal was ok
can anyone help ? many thanks Jeff2015-12-15 6:32 AM
Hello Jeff
>> I saw some thread that need to attach sys_call.c and tiny_printf.c? Is that true?
you need to add only syscalls.c that includes the_write and _read functions tiny_printf.c is a minimal implementation of printf features (like newlib-nano) : used to optimize the code size in your case you need the _write functionint
_write(
int
file,
char
*ptr,
int
len)
{
int
DataIdx;
for
(DataIdx = 0; DataIdx < len; DataIdx++)
{
__io_putchar( *ptr++ );
}
return
len;
}
then override the __io_putchar to write *ptr to USART or put the implementation within _write itself.
>> however it doesnot work.
In that case, please ensure that your USART is correctly initialized. For guidance, you can inspire from STM32CubeF1 V1.2.0\Projects\STM32VL-Discovery\Examples\UART\UART_Printf or fromSTM32F10x_StdPeriph_Lib_V3.5.0\Project\STM32F10x_StdPeriph_Examples\USART\Printf Using Standard Peripherals Library:/**
* @brief Retargets the C library printf function to the USART.
* @param None
* @retval None
*/
int
__io_putchar(
int
ch)
{
/* Place your implementation of fputc here */
/* e.g. write a character to the USART */
USART_SendData(EVAL_COM1, (uint8_t) ch);
/* Loop until the end of transmission */
while
(USART_GetFlagStatus(EVAL_COM1, USART_FLAG_TC) == RESET)
{}
return
ch;
}
Where EVAL_COM1 could be USART1 (it depends on your implementation).
Regards,
TarekB
2015-12-28 6:41 PM