cancel
Showing results for 
Search instead for 
Did you mean: 

Power down reset feature to back up the external SRAM data

vini
Associate II
Posted on April 14, 2015 at 15:33

Hi,

I want to use external SRAM with the controller STM32F429. i want to make use of internal supervisor circuit, which is used to power the internal RTC and internal 4Kb SRAM, to backup the data in external SRAM. for this i need to know following things

1. is there any GPIO with default behaviour of going low when there is PDR (power down reset)

2. is it possible to pogram any GPIO for this particular behaviour? 

Thanks

Vinay
2 REPLIES 2
Posted on April 14, 2015 at 16:57

Is power down reset the right term here?

If you're doing the SLEEP/STOP/STANDBY you'd control the GPIO pins.

There are a handful of pins documented to be in the low power domain, PC13,13,15 as I recall. Read the manual.

Other pins that lose power aren't going to stay high, Try programming a GPIO pin as output, driven high, with a pull-down low. If that doesn't work as well as you want, try a very weak external pull-down.

Look at the NRESET pin.

You're going to have to do your own experiments.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
vini
Associate II
Posted on April 15, 2015 at 06:13

Hi,

My requirement is to backup te SRAM content when there is a sudden power failure. 

is there any evk for this controller?

Thanks

Vinay