cancel
Showing results for 
Search instead for 
Did you mean: 

Power domains on STM32L552ZET6

CDan.1
Associate II

Hi guys,

I have a short question regarding the STM32L552ZET6 power domaines. Can I use 1v8 to power the chip and connect a 3v3 power supply on the VDDIO2 which I will power on from time to time(when I need to use those pins)? And another thing if I do not use the USB transceiver on MCU do I have to connect the VDDUSB to the 1v8 or leave it floating?

2 REPLIES 2
TDK
Guru

Yes, provided you comply with the powerup/powerdown restrictions:

When VDD is below 1 V, other power supplies (VDDA, VDDIO2 and VDDUSB) must remain below VDD +300 mV.

When VDD is above 1 V, all power supplies are independent.

If you feel a post has answered your question, please click "Accept as Solution".
CDan.1
Associate II

Hi,

Thank you for the answer that rule will not be a problem cause in order to get the 3v3 to the VDDIO2 pin the MCU has to be allready power-up to command 2 1v8 lines.

Thank you again.