2017-03-29 12:21 PM
I recently upgraded to a new version, 4.20, and its has been giving us a lot of issues. Unfortunately I deleted 4.18 installer, Is it possible to provide a download link to an older version of the cube?
I am working on a commercial product and things like these are a big time sink for us.
Solved! Go to Solution.
2018-07-11 06:46 PM
.
2018-07-15 02:39 AM
Thank you very much!!
2018-11-24 05:26 AM
Thank you @Community member for posting these older versions. The version 5.0.0 Graphical Interface usage is not that good as the older versions.
2018-12-09 01:55 AM
Hi,
If there is archive for more latest 4.x version (4.27.0 or above 4.20.0), I would appreciate if someone can post it here.
The speed issue of 5.0.0 is quite problematic.
Thanks!
2018-12-09 04:59 AM
They should all be there, READ and actually EXPAND the post..
2018-12-09 05:20 AM
Right! I missed the "show more" option, sorry. Thanks!
2019-01-23 07:40 AM
Hello,
Some older versions of STM32CubeMX are now available for download on ST web site.
Kind Regards,
Imen
2020-12-10 01:16 PM
I am looking for v4.3.1 of STM32CubeMx, anyone?
2020-12-10 02:25 PM
That's pretty old, does Sept-2014 seem about right?
2020-12-11 12:20 AM
Hello @Community member ,
Welcome to the STM32 Community 😊.
I recommend to you using the latest version of STM32CubeMX which contains enhancement and update, as ST maintains its support only for the latest version of STM32CubeMX available on the ST web.
Imen