cancel
Showing results for 
Search instead for 
Did you mean: 

Peripheral reset timings

Kraal
Lead

Hello,
I have a question regarding the peripheral reset registers.
For the G070 device, in the RM0454, section 5.2.16, it is specified that the clock enable of a peripheral takes 2 cycles to prevent glitches. Fine.
However, how do you experts use the reset registers ? Let's say that you want to reset the CRC peripheral.
I'm doing it like so for the moment:

RCC->AHBENR |= RCC_AHBENR_CRCEN; // Turn ON CRC peripheral clock delay_us(5); RCC->AHBRSTR = RCC_AHBRSTR_CRCRST; // Reset peripheral delay_us(5); RCC->AHBRSTR = 0; delay_us(5);

But I don't know if any delays are indeed needed or not here. Any thought on this ?

Best regards,
Kraal

3 REPLIES 3
TDK
Super User

There's no need to use the reset registers on an initial powerup as the registers will all be at their initial values.

If you feel a post has answered your question, please click "Accept as Solution".
Kraal
Lead

Thanks but that is not an answer to the question. If you jump from a bootloader to an application you might want to reset an already configured and used peripheral to its reset state.

Pavel A.
Super User

This is an interesting topic. See these threads for example:

https://community.st.com/t5/stm32-mcu-products/erratum-quot-delay-after-an-rcc-peripheral-clock-enabling-quot/m-p/580729#M220378

https://community.st.com/t5/stm32-mcu-products/inline-assembly-macro-inconsistent/m-p/580743#M220384

Bottom line: unless very restricted in time, delay for a *few* clocks. Use a reliable method for the delay.