cancel
Showing results for 
Search instead for 
Did you mean: 

PC13/PC14/PC15 pins on the STM32F103CBT6 usage

Jacek Pieczaba
Associate II

Hello,

I have a question related to the GPIOs PC13/PC14/PC15. Due to the fact that in my project I am running out of the other GPIO pins I have a question related to those pins above. I know that those pins have limitation to max 3mA sink current so do you see a problem to use them to drive LED ( I need to create a heart bit for the MCU ) where I will use LED and limit the forward current to 2-2.5mA ?

Thank you in advance

Jacek

3 REPLIES 3
Uwe Bonnes
Principal III

Use PC13-15 as Open Drain with the LED connected to VCC and you can sink current like in the other pins. If for some reason you need to source, make sure that source current for PC13-15 added does not exceed 3 mA.

Jacek Pieczaba
Associate II

Uwe,

I am really apologize for being silence for a while, but I have stuck with other work. Really appreciate for your confirmation. I am using those pins as Open Drain so simply clear.

Thank you so much

Jacek Pieczaba

Except the datasheet says it can do 3mA for sourcing and sinking. Page 64 https://www.st.com/resource/en/datasheet/stm32f103c8.pdf