2021-01-13 8:21 AM
Hello.
I want to use TIM8 instead of TIM1 to drive a WS2812B Led Strip together with DMA2 in STM32F767ZI. The code works fine with TIM1 but when I try to switch to TIM8 (which should have the same features), the interrupt handler TIM8_UP_TIM13_IRQHandler does not trigger anymore. Besides renaming everything from TIM1 to TIM8 I know I need to use TIM8_UP_TIM13 instead of TIM1_UP_TIM10 and also the strean/channel tie ins to the DMA2 also change. I have enclosed 2 pieces of code TIM1_WS2812B,c which works and TIM8_WS2812B.c where the TIM8 interrupt does not trigger. Aren't TIM1 and TIM8 suppose to work exactly the same way?
Thanks!
Solved! Go to Solution.
2021-01-14 9:47 AM
Hello! I solved it. The problem was I was using still the wrong IRQ Handler for one of the DMA streams. I fixed it and now it works! Thanks! :)
2021-01-13 8:42 AM
Troubleshoot as usually with interrupts which don't fire.
JW
2021-01-13 3:03 PM
I don't see you enable the update interrupt anywhere, in either file. HAL_TIM_Base_Start doesn't do it, and neither does __HAL_TIM_ENABLE. Could be missing something.
2021-01-14 9:47 AM
Hello! I solved it. The problem was I was using still the wrong IRQ Handler for one of the DMA streams. I fixed it and now it works! Thanks! :)