cancel
Showing results for 
Search instead for 
Did you mean: 

On 'F407, RTC Backup Registers cannot be read using SWD if RDP Level 1 is set

waclawek.jan
Super User

In STM32F407 locked to RDP Level 1, with a battery on VBAT, I keep some (not critical) data in the RTC Backup Registers.

In an attempt to investigate an incident, I tried to read out content of these registers using SWD. While I was able to read RTC registers correctly, all RTC Backup Registers read as 0 (which, according to the behaviour of program, was not true). After changing RDP to Level 0, I was able to read the correct, unperturbed content of Backup Registers.

I could not find this behaviour to be documented in RM0090.

Can ST please comment?

Thanks,

JW

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Amel NASRI
ST Employee

Hi @Community member​ ,

I need to check this & I'll come back to you.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks, Amel.

Jan

waclawek.jan
Super User

Incidentally, I've looked at RM0091 (the 'F0 RM), and there Memory protection - Read protection subchapter states:

Level 1: read protection

Debug, boot RAM and boot loader modes: In debug mode (with SWD) or when code

is running from boot RAM or boot loader, the main Flash memory and the backup

registers (RTC_BKPxR in the RTC) are totally inaccessible.

Can please ST be consistent in describing the same feature in *all* RMs.

JW

@Amel NASRI​