cancel
Showing results for 
Search instead for 
Did you mean: 

nucleof439 lwip

yang hong
Associate III

I am using nucleof439 to work Lwip, however, when I configure the project in stm32cubeide, I generate the code, and comply the project. It is fine, I also can ping the device, however, when I reenter ping command from windows cmd, the device is blocked, anybody know why?

 

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Andrew Neil
Super User

@yang hong wrote:

 when I reenter ping command from windows cmd, the device is blocked


What do you mean by that?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
ST Employee

Hello,

Do you mean that the ping success only once and the second ping has no response?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.