cancel
Showing results for 
Search instead for 
Did you mean: 

nucleof439 lwip

yang hong
Associate II

I am using nucleof439 to work Lwip, however, when I configure the project in stm32cubeide, I generate the code, and comply the project. It is fine, I also can ping the device, however, when I reenter ping command from windows cmd, the device is blocked, anybody know why?

 

2 REPLIES 2
Andrew Neil
Evangelist III

@yang hong wrote:

 when I reenter ping command from windows cmd, the device is blocked


What do you mean by that?

SofLit
ST Employee

Hello,

Do you mean that the ping success only once and the second ping has no response?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.