cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-H745ZI-Q DMA Problem

EsonShen
Associate II

I tried to use this board to capture image by using DCMI DMA with a ov2640 camera. The problem is data read is successful in DCMI(by watching the register) but the buffer(initialized:uint32_t buffer[16000]={0}) used to store the image data was the same as it was initialized. I think this is a DMA problem.Register after running"HAL_DCMI_Start_DMA"Register after running"HAL_DCMI_Start_DMA"buffer(HEX) sent via USART after "HAL_DCMI_Stop"buffer(HEX) sent via USART after "HAL_DCMI_Stop"

 

/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2024 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" #include "string.h" #include <stdio.h> /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ #include "ov2640.h" /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ #ifndef HSEM_ID_0 #define HSEM_ID_0 (0U) /* HW semaphore 0*/ #endif /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ #if defined ( __ICCARM__ ) /*!< IAR Compiler */ #pragma location=0x30000000 ETH_DMADescTypeDef DMARxDscrTab[ETH_RX_DESC_CNT]; /* Ethernet Rx DMA Descriptors */ #pragma location=0x30000080 ETH_DMADescTypeDef DMATxDscrTab[ETH_TX_DESC_CNT]; /* Ethernet Tx DMA Descriptors */ #elif defined ( __CC_ARM ) /* MDK ARM Compiler */ __attribute__((at(0x30000000))) ETH_DMADescTypeDef DMARxDscrTab[ETH_RX_DESC_CNT]; /* Ethernet Rx DMA Descriptors */ __attribute__((at(0x30000080))) ETH_DMADescTypeDef DMATxDscrTab[ETH_TX_DESC_CNT]; /* Ethernet Tx DMA Descriptors */ #elif defined ( __GNUC__ ) /* GNU Compiler */ ETH_DMADescTypeDef DMARxDscrTab[ETH_RX_DESC_CNT] __attribute__((section(".RxDecripSection"))); /* Ethernet Rx DMA Descriptors */ ETH_DMADescTypeDef DMATxDscrTab[ETH_TX_DESC_CNT] __attribute__((section(".TxDecripSection"))); /* Ethernet Tx DMA Descriptors */ #endif ETH_TxPacketConfig TxConfig; DCMI_HandleTypeDef hdcmi; DMA_HandleTypeDef hdma_dcmi; ETH_HandleTypeDef heth; UART_HandleTypeDef huart3; /* USER CODE BEGIN PV */ HAL_StatusTypeDef dcmi_dma_status = HAL_OK; uint8_t ov2640_verh = 0xff, ov2640_verl=0xff; uint32_t dcmi_data_buff[16000]; uint32_t DCMI_RN = 0; //row number uint32_t DCMI_CN = 0; //column number uint32_t DCMI_RS = 0; //row start uint32_t DCMI_CS = 0; //column start uint8_t tx_busy = 0; /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_DMA_Init(void); static void MX_DCMI_Init(void); static void MX_ETH_Init(void); static void MX_USART3_UART_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ #define PUTCHAR_PROTOTYPE int fputc(int ch, FILE *f) PUTCHAR_PROTOTYPE { USART3->TDR = ch; while(!(USART3->ISR& USART_ISR_TXE_TXFNF_Msk)) {;} return ch; } void Send(uint8_t *pData,int jpglen) { uint32_t i = 0; //printf("jpeg data size:%d\r\n",JPEG_BUFFER_LENGTH); HAL_Delay(1000); for(i = 0;i < jpglen;i++) { //printf("%02x\t",pData[i]); printf("%c",pData[i]); } HAL_Delay(1000); printf("\r\n"); } void PY_OV2640_RGB565_CONFIG(void) { /*Camera Interface*/ SCCB_Rst(); //hard reset HAL_Delay(100); SCCB_WR_Reg(0xff, 0x01); //soft reset SCCB_WR_Reg(0x12, 0x80); HAL_Delay(100); ov2640_verh = SCCB_RD_Reg(0x1c); HAL_Delay(50); ov2640_verl = SCCB_RD_Reg(0x1d); HAL_Delay(50); while ((ov2640_verh==0xff)||(ov2640_verl==0xff)) { HAL_UART_Transmit(&huart3, &ov2640_verh, 1, 0xFFFFFF); HAL_Delay(500); HAL_UART_Transmit(&huart3, &ov2640_verl, 1, 0xFFFFFF); HAL_Delay(500); } OV2640_UXGA_Init(); //pix speed adjustment SCCB_WR_Reg(0xff, 0x00); SCCB_WR_Reg(0xd3, 0x00); SCCB_WR_Reg(0XFF, 0X01); SCCB_WR_Reg(0X11, 0x01); OV2640_RGB565_Mode(); OV2640_OutSize_Set(640, 480); HAL_Delay(200); } void getStatus(void){ HAL_DCMI_StateTypeDef State = HAL_DCMI_GetState(&hdcmi); uint32_t Error = HAL_DCMI_GetError(&hdcmi); printf("DCMI State: %ld, Error: %ld\r\n", (long)State, (long)Error); HAL_DMA_StateTypeDef DMA_State = HAL_DMA_GetState(&hdma_dcmi); uint32_t DMA_Error = HAL_DMA_GetError(&hdma_dcmi); printf("DMA State: %d, Error: %ld\r\n", DMA_State, (long)DMA_Error); HAL_Delay(10000); } /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* USER CODE BEGIN Boot_Mode_Sequence_0 */ int32_t timeout; /* USER CODE END Boot_Mode_Sequence_0 */ /* USER CODE BEGIN Boot_Mode_Sequence_1 */ /* Wait until CPU2 boots and enters in stop mode or timeout*/ timeout = 0xFFFF; while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) != RESET) && (timeout-- > 0)); if ( timeout < 0 ) { Error_Handler(); } /* USER CODE END Boot_Mode_Sequence_1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN Boot_Mode_Sequence_2 */ /* When system initialization is finished, Cortex-M7 will release Cortex-M4 by means of HSEM notification */ /*HW semaphore Clock enable*/ __HAL_RCC_HSEM_CLK_ENABLE(); /*Take HSEM */ HAL_HSEM_FastTake(HSEM_ID_0); /*Release HSEM in order to notify the CPU2(CM4)*/ HAL_HSEM_Release(HSEM_ID_0,0); /* wait until CPU2 wakes up from stop mode */ timeout = 0xFFFF; while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) == RESET) && (timeout-- > 0)); if ( timeout < 0 ) { Error_Handler(); } /* USER CODE END Boot_Mode_Sequence_2 */ /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_DMA_Init(); MX_DCMI_Init(); MX_ETH_Init(); MX_USART3_UART_Init(); /* USER CODE BEGIN 2 */ PY_OV2640_RGB565_CONFIG(); /* USER CODE END 2 */ uint8_t id = SCCB_RD_Reg(0x00); printf("id :%did",id); HAL_Delay(10000); /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ printf("1\n"); getStatus(); dcmi_dma_status = HAL_DCMI_Init(&hdcmi); printf("2\n"); getStatus(); for (uint8_t i=0; i<10;i++) { // HAL_DCMI_DisableCrop (&hdcmi); DCMI_RN = 48; DCMI_CN = 1280; DCMI_RS = 48*i; DCMI_CS = 0; // HAL_DCMI_ConfigCrop (&hdcmi, DCMI_CS, DCMI_RS, DCMI_CN, DCMI_RN); // HAL_Delay(1); // HAL_DCMI_EnableCrop (&hdcmi); // HAL_Delay(1); printf("3\n"); getStatus(); HAL_DCMI_Stop(&hdcmi); printf("4\n"); getStatus(); MX_DCMI_Init(); printf("5\n"); getStatus(); __HAL_DCMI_ENABLE_IT(&hdcmi, DCMI_IT_FRAME); dcmi_dma_status = HAL_DCMI_Start_DMA(&hdcmi, DCMI_MODE_CONTINUOUS, (uint32_t)&dcmi_data_buff, DCMI_CN*DCMI_RN/4); printf("6\n"); getStatus(); while(HAL_DMA_GetState(&hdma_dcmi)==HAL_DMA_STATE_BUSY) ; //HAL_DCMI_Resume(&hdcmi); HAL_DCMI_Stop(&hdcmi); tx_busy = 1; Send((uint8_t *)dcmi_data_buff, 61440); HAL_Delay(1000000); while(tx_busy!=0) ; } } /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Configure the main internal regulator output voltage */ __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3); // ???????????? RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK) { Error_Handler(); } // ?????? RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 8; RCC_OscInitStruct.PLL.PLLN = 336; RCC_OscInitStruct.PLL.PLLP = 2; RCC_OscInitStruct.PLL.PLLQ = 7; RCC_OscInitStruct.PLL.PLLR = 2; RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_1; RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE; RCC_OscInitStruct.PLL.PLLFRACN = 0; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } // ???????????,????????????? RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2 |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2; RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK) { Error_Handler(); } HAL_RCC_MCOConfig(RCC_MCO1, RCC_MCO1SOURCE_HSI, RCC_MCODIV_8); // ???????? RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSIState = RCC_HSI_OFF; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } } /** * @brief DCMI Initialization Function * @PAram None * @retval None */ static void MX_DCMI_Init(void) { /* USER CODE BEGIN DCMI_Init 0 */ /* USER CODE END DCMI_Init 0 */ /* USER CODE BEGIN DCMI_Init 1 */ /* USER CODE END DCMI_Init 1 */ hdcmi.Instance = DCMI; hdcmi.Init.SynchroMode = DCMI_SYNCHRO_HARDWARE; hdcmi.Init.PCKPolarity = DCMI_PCKPOLARITY_RISING; hdcmi.Init.VSPolarity = DCMI_VSPOLARITY_LOW; hdcmi.Init.HSPolarity = DCMI_HSPOLARITY_LOW; hdcmi.Init.CaptureRate = DCMI_CR_ALL_FRAME; hdcmi.Init.ExtendedDataMode = DCMI_EXTEND_DATA_8B; hdcmi.Init.JPEGMode = DCMI_JPEG_ENABLE; hdcmi.Init.ByteSelectMode = DCMI_BSM_ALL; hdcmi.Init.ByteSelectStart = DCMI_OEBS_ODD; hdcmi.Init.LineSelectMode = DCMI_LSM_ALL; hdcmi.Init.LineSelectStart = DCMI_OELS_ODD; if (HAL_DCMI_Init(&hdcmi) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN DCMI_Init 2 */ /* USER CODE END DCMI_Init 2 */ } /** * @brief ETH Initialization Function * @PAram None * @retval None */ static void MX_ETH_Init(void) { /* USER CODE BEGIN ETH_Init 0 */ /* USER CODE END ETH_Init 0 */ static uint8_t MACAddr[6]; /* USER CODE BEGIN ETH_Init 1 */ /* USER CODE END ETH_Init 1 */ heth.Instance = ETH; MACAddr[0] = 0x00; MACAddr[1] = 0x80; MACAddr[2] = 0xE1; MACAddr[3] = 0x00; MACAddr[4] = 0x00; MACAddr[5] = 0x00; heth.Init.MACAddr = &MACAddr[0]; heth.Init.MediaInterface = HAL_ETH_RMII_MODE; heth.Init.TxDesc = DMATxDscrTab; heth.Init.RxDesc = DMARxDscrTab; heth.Init.RxBuffLen = 1524; /* USER CODE BEGIN MACADDRESS */ /* USER CODE END MACADDRESS */ if (HAL_ETH_Init(&heth) != HAL_OK) { Error_Handler(); } memset(&TxConfig, 0 , sizeof(ETH_TxPacketConfig)); TxConfig.Attributes = ETH_TX_PACKETS_FEATURES_CSUM | ETH_TX_PACKETS_FEATURES_CRCPAD; TxConfig.ChecksumCtrl = ETH_CHECKSUM_IPHDR_PAYLOAD_INSERT_PHDR_CALC; TxConfig.CRCPadCtrl = ETH_CRC_PAD_INSERT; /* USER CODE BEGIN ETH_Init 2 */ /* USER CODE END ETH_Init 2 */ } /** * @brief USART3 Initialization Function * @PAram None * @retval None */ static void MX_USART3_UART_Init(void) { /* USER CODE BEGIN USART3_Init 0 */ /* USER CODE END USART3_Init 0 */ /* USER CODE BEGIN USART3_Init 1 */ /* USER CODE END USART3_Init 1 */ huart3.Instance = USART3; huart3.Init.BaudRate = 115200; huart3.Init.WordLength = UART_WORDLENGTH_8B; huart3.Init.StopBits = UART_STOPBITS_1; huart3.Init.Parity = UART_PARITY_NONE; huart3.Init.Mode = UART_MODE_TX_RX; huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart3.Init.OverSampling = UART_OVERSAMPLING_16; huart3.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; huart3.Init.ClockPrescaler = UART_PRESCALER_DIV1; huart3.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; if (HAL_UART_Init(&huart3) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetTxFifoThreshold(&huart3, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetRxFifoThreshold(&huart3, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_DisableFifoMode(&huart3) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USART3_Init 2 */ /* USER CODE END USART3_Init 2 */ } /** * Enable DMA controller clock */ static void MX_DMA_Init(void) { /* DMA controller clock enable */ __HAL_RCC_DMA1_CLK_ENABLE(); HAL_DMA_Init(&hdma_dcmi) ; /* DMA interrupt init */ /* DMA1_Stream0_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Stream0_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Stream0_IRQn); } /** * @brief GPIO Initialization Function * @PAram None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOE_CLK_ENABLE(); __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOH_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); __HAL_RCC_GPIOD_CLK_ENABLE(); __HAL_RCC_GPIOG_CLK_ENABLE(); /*Configure GPIO pins : PA11 PA12 */ GPIO_InitStruct.Pin = GPIO_PIN_11|GPIO_PIN_12; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF10_OTG1_FS; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /* USER CODE BEGIN MX_GPIO_Init_2 */ /*Configure GPIO pins : PB6 PB7 */ GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); /*Configure GPIO pins : PD12 PD13 */ GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_13; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOD, &GPIO_InitStruct); OV2640_PWUP; OV2640_RUN; /*Configure GPIO pin : PA8 */ GPIO_InitStruct.Pin = GPIO_PIN_8; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF0_MCO; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @PAram file: pointer to the source file name * @PAram line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */
View more

 

 

3 REPLIES 3
TDK
Guru

Ensure that dcmi_data_buff is not in DTCM and is somewhere the DMA can access.

While debugging the program, after the transfer should have taken plane, look at the DMA registers to see if an error occurred.

Data cache coherency might also be an issue in the future, although it's not the main culprit here. I suggest disabling it during the debugging stage.

 

If you feel a post has answered your question, please click "Accept as Solution".

Thank you for your solution, this problem has been solved but not still correctly get the image. But over all thank you!

Unfortunately I found it does not really work.I use "uint32_t dcmi_data_buff[2560] __attribute__((section(".ARM.__at_0x24040000")));" to give buffer a location DMA can reach.

屏幕截图 2024-08-05 170722.png

but the content of buffer after HAL_DCMI_Start _DMA is the same as it was before HAL_DCMI_Start_DMA.I think the data I get is the original data in this location. Am I Wrong?

main.c:

/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2024 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" #include "string.h" #include <stdio.h> /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ #include "ov2640.h" /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ #define JPEG_BUFFER_LENGTH 10*1024/4 #define USART_BUFFER_LENGTH JPEG_BUFFER_LENGTH*4 #define JPEG_BUFFER_NUM 2 #define JPEG_WIDTH 1600 #define JPEG_HEIGHT 1200 /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ #ifndef HSEM_ID_0 #define HSEM_ID_0 (0U) /* HW semaphore 0*/ #endif /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ #if defined ( __ICCARM__ ) /*!< IAR Compiler */ #pragma location=0x30000000 ETH_DMADescTypeDef DMARxDscrTab[ETH_RX_DESC_CNT]; /* Ethernet Rx DMA Descriptors */ #pragma location=0x30000080 ETH_DMADescTypeDef DMATxDscrTab[ETH_TX_DESC_CNT]; /* Ethernet Tx DMA Descriptors */ #elif defined ( __CC_ARM ) /* MDK ARM Compiler */ __attribute__((at(0x30000000))) ETH_DMADescTypeDef DMARxDscrTab[ETH_RX_DESC_CNT]; /* Ethernet Rx DMA Descriptors */ __attribute__((at(0x30000080))) ETH_DMADescTypeDef DMATxDscrTab[ETH_TX_DESC_CNT]; /* Ethernet Tx DMA Descriptors */ #elif defined ( __GNUC__ ) /* GNU Compiler */ ETH_DMADescTypeDef DMARxDscrTab[ETH_RX_DESC_CNT] __attribute__((section(".RxDecripSection"))); /* Ethernet Rx DMA Descriptors */ ETH_DMADescTypeDef DMATxDscrTab[ETH_TX_DESC_CNT] __attribute__((section(".TxDecripSection"))); /* Ethernet Tx DMA Descriptors */ #endif ETH_TxPacketConfig TxConfig; DCMI_HandleTypeDef hdcmi; DMA_HandleTypeDef hdma_dcmi; ETH_HandleTypeDef heth; UART_HandleTypeDef huart3; /* USER CODE BEGIN PV */ HAL_StatusTypeDef dcmi_dma_status = HAL_OK; uint8_t ov2640_verh = 0xff, ov2640_verl=0xff; uint32_t dcmi_data_buff[2560] __attribute__((section(".ARM.__at_0x24040000"))); uint32_t DCMI_RN = 0; //row number uint32_t DCMI_CN = 0; //column number uint32_t DCMI_RS = 0; //row start uint32_t DCMI_CS = 0; //column start uint8_t tx_busy = 0; /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_DMA_Init(void); static void MX_DCMI_Init(void); static void MX_ETH_Init(void); static void MX_USART3_UART_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ #define PUTCHAR_PROTOTYPE int fputc(int ch, FILE *f) PUTCHAR_PROTOTYPE { USART3->TDR = ch; while(!(USART3->ISR& USART_ISR_TXE_TXFNF_Msk)) {;} return ch; } void Send(uint8_t *pData,int jpglen) { uint32_t i = 0; //printf("jpeg data size:%d\r\n",JPEG_BUFFER_LENGTH); HAL_Delay(1000); for(i = 0;i < jpglen;i++) { //printf("%02x\t",pData[i]); printf("%c",pData[i]); } HAL_Delay(1000); printf("\r\n"); } void PY_OV2640_RGB565_CONFIG(void) { /*Camera Interface*/ SCCB_Rst(); //hard reset HAL_Delay(100); SCCB_WR_Reg(0xff, 0x01); //soft reset SCCB_WR_Reg(0x12, 0x80); HAL_Delay(100); ov2640_verh = SCCB_RD_Reg(0x1c); HAL_Delay(50); ov2640_verl = SCCB_RD_Reg(0x1d); HAL_Delay(50); while ((ov2640_verh==0xff)||(ov2640_verl==0xff)) { HAL_UART_Transmit(&huart3, &ov2640_verh, 1, 0xFFFFFF); HAL_Delay(500); HAL_UART_Transmit(&huart3, &ov2640_verl, 1, 0xFFFFFF); HAL_Delay(500); } OV2640_UXGA_Init(); //pix speed adjustment SCCB_WR_Reg(0xff, 0x00); SCCB_WR_Reg(0xd3, 0x00); SCCB_WR_Reg(0XFF, 0X01); SCCB_WR_Reg(0X11, 0x01); //OV2640_RGB565_Mode(); OV2640_JPEG_Mode(); OV2640_OutSize_Set(640, 480); HAL_Delay(200); } /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* USER CODE BEGIN Boot_Mode_Sequence_0 */ int32_t timeout; /* USER CODE END Boot_Mode_Sequence_0 */ /* USER CODE BEGIN Boot_Mode_Sequence_1 */ /* Wait until CPU2 boots and enters in stop mode or timeout*/ timeout = 0xFFFF; while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) != RESET) && (timeout-- > 0)); if ( timeout < 0 ) { Error_Handler(); } /* USER CODE END Boot_Mode_Sequence_1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN Boot_Mode_Sequence_2 */ /* When system initialization is finished, Cortex-M7 will release Cortex-M4 by means of HSEM notification */ /*HW semaphore Clock enable*/ __HAL_RCC_HSEM_CLK_ENABLE(); /*Take HSEM */ HAL_HSEM_FastTake(HSEM_ID_0); /*Release HSEM in order to notify the CPU2(CM4)*/ HAL_HSEM_Release(HSEM_ID_0,0); /* wait until CPU2 wakes up from stop mode */ timeout = 0xFFFF; while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) == RESET) && (timeout-- > 0)); if ( timeout < 0 ) { Error_Handler(); } /* USER CODE END Boot_Mode_Sequence_2 */ /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_DMA_Init(); MX_DCMI_Init(); MX_ETH_Init(); MX_USART3_UART_Init(); /* USER CODE BEGIN 2 */ //PY_OV2640_RGB565_CONFIG(); /* USER CODE END 2 */ OV2640_Init(); OV2640_RGB565_Mode(); OV2640_JPEG_Mode(); OV2640_Light_Mode(0); OV2640_OutSize_Set(JPEG_WIDTH,JPEG_HEIGHT); HAL_Delay(10); /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ dcmi_dma_status = HAL_DCMI_Init(&hdcmi); // ??DCMI?? HAL_DCMI_StateTypeDef State = HAL_DCMI_GetState(&hdcmi); uint32_t Error = HAL_DCMI_GetError(&hdcmi); Send((uint8_t *)dcmi_data_buff, sizeof(dcmi_data_buff)); HAL_Delay(10000); // ??DCMI??????? printf("DCMI State: %ld, Error: %ld\r\n", (long)State, (long)Error); // ??DMA?? HAL_DMA_StateTypeDef DMA_State = HAL_DMA_GetState(&hdma_dcmi); uint32_t DMA_Error = HAL_DMA_GetError(&hdma_dcmi); // ??DMA??????? printf("DMA State: %d, Error: %ld\r\n", DMA_State, (long)DMA_Error); HAL_Delay(1000); for (uint8_t i=0; i<10;i++) { // HAL_DCMI_DisableCrop (&hdcmi); // DCMI_RN = 48; // DCMI_CN = 1280; // DCMI_RS = 48*i; // DCMI_CS = 0; // HAL_DCMI_ConfigCrop (&hdcmi, DCMI_CS, DCMI_RS, DCMI_CN, DCMI_RN); // HAL_Delay(1); // HAL_DCMI_EnableCrop (&hdcmi); // HAL_Delay(1); HAL_DCMI_Stop(&hdcmi); MX_DCMI_Init(); __HAL_DCMI_ENABLE_IT(&hdcmi, DCMI_IT_FRAME); dcmi_dma_status = HAL_DCMI_Start_DMA(&hdcmi, DCMI_MODE_CONTINUOUS, (uint32_t)&dcmi_data_buff, DCMI_CN*DCMI_RN/4); while(HAL_DMA_GetState(&hdma_dcmi)==HAL_DMA_STATE_BUSY) ; //HAL_DCMI_Resume(&hdcmi); HAL_DCMI_Stop(&hdcmi); tx_busy = 1; Send((uint8_t *)dcmi_data_buff, sizeof(dcmi_data_buff)); HAL_Delay(1000000); while(tx_busy!=0) ; } } /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Configure the main internal regulator output voltage */ __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3); // ???????????? RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK) { Error_Handler(); } // ?????? RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 8; RCC_OscInitStruct.PLL.PLLN = 336; RCC_OscInitStruct.PLL.PLLP = 2; RCC_OscInitStruct.PLL.PLLQ = 7; RCC_OscInitStruct.PLL.PLLR = 2; RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_1; RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE; RCC_OscInitStruct.PLL.PLLFRACN = 0; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } // ???????????,????????????? RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2 |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2; RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK) { Error_Handler(); } HAL_RCC_MCOConfig(RCC_MCO1, RCC_MCO1SOURCE_HSI, RCC_MCODIV_8); // ???????? RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSIState = RCC_HSI_OFF; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } } /** * @brief DCMI Initialization Function * @PAram None * @retval None */ static void MX_DCMI_Init(void) { /* USER CODE BEGIN DCMI_Init 0 */ /* USER CODE END DCMI_Init 0 */ /* USER CODE BEGIN DCMI_Init 1 */ /* USER CODE END DCMI_Init 1 */ hdcmi.Instance = DCMI; hdcmi.Init.SynchroMode = DCMI_SYNCHRO_HARDWARE; hdcmi.Init.PCKPolarity = DCMI_PCKPOLARITY_RISING; hdcmi.Init.VSPolarity = DCMI_VSPOLARITY_LOW; hdcmi.Init.HSPolarity = DCMI_HSPOLARITY_LOW; hdcmi.Init.CaptureRate = DCMI_CR_ALL_FRAME; hdcmi.Init.ExtendedDataMode = DCMI_EXTEND_DATA_8B; hdcmi.Init.JPEGMode = DCMI_JPEG_ENABLE; hdcmi.Init.ByteSelectMode = DCMI_BSM_ALL; hdcmi.Init.ByteSelectStart = DCMI_OEBS_ODD; hdcmi.Init.LineSelectMode = DCMI_LSM_ALL; hdcmi.Init.LineSelectStart = DCMI_OELS_ODD; if (HAL_DCMI_Init(&hdcmi) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN DCMI_Init 2 */ /* USER CODE END DCMI_Init 2 */ } /** * @brief ETH Initialization Function * @PAram None * @retval None */ static void MX_ETH_Init(void) { /* USER CODE BEGIN ETH_Init 0 */ /* USER CODE END ETH_Init 0 */ static uint8_t MACAddr[6]; /* USER CODE BEGIN ETH_Init 1 */ /* USER CODE END ETH_Init 1 */ heth.Instance = ETH; MACAddr[0] = 0x00; MACAddr[1] = 0x80; MACAddr[2] = 0xE1; MACAddr[3] = 0x00; MACAddr[4] = 0x00; MACAddr[5] = 0x00; heth.Init.MACAddr = &MACAddr[0]; heth.Init.MediaInterface = HAL_ETH_RMII_MODE; heth.Init.TxDesc = DMATxDscrTab; heth.Init.RxDesc = DMARxDscrTab; heth.Init.RxBuffLen = 1524; /* USER CODE BEGIN MACADDRESS */ /* USER CODE END MACADDRESS */ if (HAL_ETH_Init(&heth) != HAL_OK) { Error_Handler(); } memset(&TxConfig, 0 , sizeof(ETH_TxPacketConfig)); TxConfig.Attributes = ETH_TX_PACKETS_FEATURES_CSUM | ETH_TX_PACKETS_FEATURES_CRCPAD; TxConfig.ChecksumCtrl = ETH_CHECKSUM_IPHDR_PAYLOAD_INSERT_PHDR_CALC; TxConfig.CRCPadCtrl = ETH_CRC_PAD_INSERT; /* USER CODE BEGIN ETH_Init 2 */ /* USER CODE END ETH_Init 2 */ } /** * @brief USART3 Initialization Function * @PAram None * @retval None */ static void MX_USART3_UART_Init(void) { /* USER CODE BEGIN USART3_Init 0 */ /* USER CODE END USART3_Init 0 */ /* USER CODE BEGIN USART3_Init 1 */ /* USER CODE END USART3_Init 1 */ huart3.Instance = USART3; huart3.Init.BaudRate = 115200; huart3.Init.WordLength = UART_WORDLENGTH_8B; huart3.Init.StopBits = UART_STOPBITS_1; huart3.Init.Parity = UART_PARITY_NONE; huart3.Init.Mode = UART_MODE_TX_RX; huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart3.Init.OverSampling = UART_OVERSAMPLING_16; huart3.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; huart3.Init.ClockPrescaler = UART_PRESCALER_DIV1; huart3.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; if (HAL_UART_Init(&huart3) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetTxFifoThreshold(&huart3, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetRxFifoThreshold(&huart3, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_DisableFifoMode(&huart3) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USART3_Init 2 */ /* USER CODE END USART3_Init 2 */ } /** * Enable DMA controller clock */ static void MX_DMA_Init(void) { /* DMA controller clock enable */ __HAL_RCC_DMA1_CLK_ENABLE(); HAL_DMA_Init(&hdma_dcmi) ; /* DMA interrupt init */ /* DMA1_Stream0_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Stream0_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Stream0_IRQn); } /** * @brief GPIO Initialization Function * @PAram None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOE_CLK_ENABLE(); __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOH_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); __HAL_RCC_GPIOD_CLK_ENABLE(); __HAL_RCC_GPIOG_CLK_ENABLE(); /*Configure GPIO pins : PA11 PA12 */ GPIO_InitStruct.Pin = GPIO_PIN_11|GPIO_PIN_12; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF10_OTG1_FS; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /* USER CODE BEGIN MX_GPIO_Init_2 */ /*Configure GPIO pins : PB6 PB7 */ GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); /*Configure GPIO pins : PD12 PD13 */ GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_13; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOD, &GPIO_InitStruct); OV2640_PWUP; OV2640_RUN; /*Configure GPIO pin : PA8 */ GPIO_InitStruct.Pin = GPIO_PIN_8; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF0_MCO; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @PAram file: pointer to the source file name * @PAram line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */
View more