2024-11-30 08:10 PM
Make dual data line SPI running on nucleo-H743zi2, using SPI-2 as master and SPI-3 slave.
Solved! Go to Solution.
2024-12-01 03:19 AM
After brief review of AN4760, I get an impression that QuadSPI was specificaly designed to interface Flash memory IC.
ADC has absolutely different requirements in respect to timing on CS line, clock - 32 SCLK clocks with 16 data bits.
See pictures:
2024-11-30 11:37 PM - edited 2024-11-30 11:38 PM
Why no QSPI ?
2024-12-01 03:19 AM
After brief review of AN4760, I get an impression that QuadSPI was specificaly designed to interface Flash memory IC.
ADC has absolutely different requirements in respect to timing on CS line, clock - 32 SCLK clocks with 16 data bits.
See pictures: