cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H745 maximum sample rate

mosamasa
Visitor

Hi,

I'm looking for baseband processor for my IQ receiver. I would need dual 12-bit ADC with 5.12MSPS rate. I hope to get data from two ADC to DMA syncronously.

I have been looking for STM32H745 for this task. Based on the datasheet, maximum sample rate is 5.5MSPS. It seems that value is given for package UFBGA176+25. I would prefer to use LQFP144 package. Based on AN5354, I can only get 3.63MSPS (12 bit) sample rate.

Is there any way to overcome this issue or do I have to use BGA version?

0 REPLIES 0