cancel
Showing results for 
Search instead for 
Did you mean: 

How to receive a number, add a number to it and transmit it again?

222student
Associate

I am trying to add 5 to the received number but I can't figure out what am I doing wrong.
This is the code from Keil

 

uint8_t receivedNumber;
uint8_t newNumber;

while(1){
if(HAL_UART_Receive_IT(&huart2,(uint8_t *)&receivedNumber,sizeof(receivedNumber))==HAL_OK)
{
 int newNumber=receivedNumber+5;
 HAL_UART_Transmit(&huart2,(uint8_t *)&newNumber,sizeof(newNumber),1000);
}
}

 

When it receives 1,2,3 or 4, it transmits 6,7,8,9 (as expected). When it receives 5 it transmits a " : "  and when it receives 11,21,37 or 42, it transmits 66,76,8< and 97.
Edit:5,6,7,8 to 6,7,8,9

3 REPLIES 3
Peter BENSCH
ST Employee

Welcome @222student, to the community!

Please read through the coding of characters again (keyword ASCII table). What you are receiving are ASCII characters that cannot be readily calculated.

Incidentally, "5" is not an expected output if you have received "1" and add 5 - is it?

In any case, the (ASCII) character "1" is encoded in binary 0x31. If you add 5, you get 0x36, which corresponds to the character "6" in the ASCII table. However, if you receive, for example, the character "5" with the ASCII equivalent of 0x35, your calculation results in 0x3A, which stands for the character ":".

You must therefore pay attention to WHAT you are receiving and how it is to be INTERPRETED.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you so much for the reply, I will look into it.

And yeah, I meant "6,7,8,9" not "5,6,7,8"

Perhaps ponder how integer number space vs ASCII works.

Look at sscanf() and sprintf()

Look at atoi() and itoa()

 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..