2025-02-17 5:31 AM - last edited on 2025-03-06 6:41 AM by Peter BENSCH
Hi everyone,
I am having issues interfacing an ADS1298 board with a NUCLEO F767ZI.
void ADS1298_ReadConfig1(SPI_HandleTypeDef *hspi) {
uint8_t command[2] = {0x20 | 0x00, 0x00}; // RREG command for sending ID
uint8_t sdatacCmd = 0x11; // SDATAC mode command for sending data
GPIOA->BSRR = GPIO_BSRR_BR4; // CS LOW
*(volatile uint8_t *)&SPI1->DR = sdatacCmd; // SDATAC command, stop reading data so the ADS1298 can receive commands -- direct register access method
while (!(SPI1->SR & SPI_SR_TXE)); // Wait until TXE (Transmit buffer empty) is set
while (SPI1->SR & SPI_SR_BSY); // Wait for transmission to complete
while (!(SPI1->SR & SPI_SR_RXNE)); // Wait until RXNE (Receive buffer empty) is set
volatile uint8_t sdatac_status = *(volatile uint8_t *)&SPI1->DR; // Discard
*(volatile uint8_t *)&SPI1->DR = command[0];
while (!(SPI1->SR & SPI_SR_TXE));
while (SPI1->SR & SPI_SR_BSY);
while (!(SPI1->SR & SPI_SR_RXNE));
volatile uint8_t rreg_status1 = *(volatile uint8_t *)&SPI1->DR; // Discard
*(volatile uint8_t *)&SPI1->DR = command[1];
while (!(SPI1->SR & SPI_SR_TXE));
while (SPI1->SR & SPI_SR_BSY);
while (!(SPI1->SR & SPI_SR_RXNE));
volatile uint8_t rreg_status2 = *(volatile uint8_t *)&SPI1->DR; // Discard
*(volatile uint8_t *)&SPI1->DR = 0xFF; // Dummy byte
while (!(SPI1->SR & SPI_SR_TXE));
while (SPI1->SR & SPI_SR_BSY);
while (!(SPI1->SR & SPI_SR_RXNE));
response = *(volatile uint8_t *)&SPI1->DR; // Save ID in a buffer
for ( int i = 0; i < 10; i++); // Small delay to have >2 us between last CLK falling edge and CS high
GPIOA->BSRR = GPIO_BSRR_BS4; // CS HIGH
printf("CONFIG1: 0x%02X\n", response);
}
I set DRDY (data ready pin) as an interrupt, meaning that this function runs every time DRDY toggles. It seems like I am getting the correct ID 0x92 at address 0x20 | 0x00, but for some reason I am also reading the CONFIG1 register 0x86 which is 0x20 | 0x01 at the beginning of each new SPI transaction. From the printf function I see CONFIG1: 0x86, even though it should be 0x92.
I thought I am flushing the FIFO by reading the buffer each time I send a byte. Does anyone have any suggestions on what could cause the extra byte at the beginning of the SPI transactions? I also asked on the TI forums as it might be more ADS1298 related than the STM32 NUCLEO board.