Nucleo F401RE Usart Tx Blink Led
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-08 10:46 PM
I have Nucleo F401RE board.
I want to Turn On Led When Usart Tx pin high and Turn Off When Usart Tx pin is low.
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
uint8_t data_tx[5] = {0x41 , 0x42 ,0x43 ,0x44 , 0x45};
uint8_t data_rx[5];
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_USART2_UART_Init();
MX_USART1_UART_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
//HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
//hdma_usart1_tx.Instance->CR |= (1<<0);
//HAL_UART_Receive_DMA(&huart1, data_rx, 5);
HAL_UART_Transmit_DMA(&huart1, data_tx, 5);
if((GPIOA->ODR & GPIO_PIN_9)==1 | (GPIOA->ODR & GPIO_PIN_10)==1)
{
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin , 1);
}else
{
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin , 0);
}
//HAL_GPIO_ReadPin(LD2_GPIO_Port, LD2_Pin);
//HAL_Delay(50);
}
/* USER CODE END 3 */
}
The code is above and I always read Tx Pin low...
Is there any other way or solution?
Solved! Go to Solution.
- Labels:
-
STM32F4 Series
-
UART-USART
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-09 5:27 AM
I don't know, you have to dig the reference manual.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-09 1:23 AM
if you use a mask to check a bit you must compare against 0 not 1: if ((GPIOA->ODR & mask) != 0)
If the bit you check is not the LSB the result will not be 1...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-09 4:33 AM
Hi Nikita ,
it's my mistake thank you so much.
Actually I change like below just a test . But GPIOA-> ODR data always zero doesnt change.
USART1 TX pin is connnected PA9... And it transmit data. But GPIOA-> ODR value doesnt change.
I think GPIO ode in AF mode doesnt change ODR register status. Is there any way to read Pin state in AF Mode ????
if(GPIOA->ODR != 0)
{
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin , 1);
}else
{
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin , 0);
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-09 5:27 AM
I don't know, you have to dig the reference manual.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-09 5:32 AM
In the Referance manual , it 's written . Below code Works For Nucleo F401RE
if((GPIOA->IDR & GPIO_PIN_9)!= 0)
{
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin , 0);
}else
{
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin , 1);
}