Associate II
February 23, 2023
Question
NUCLEO-C031C6 upates adc value only once upon start up but does not update afterwards
- February 23, 2023
- 3 replies
- 3749 views
I am working with a NUCLEO-C031C6 board using STM32Cube ide V1.11.0 and I am noticing something weird with my ADC readings, I am using PA0 and PA1 for AIN0 and AIN1 when I launch the application I get the correct value if I have a signal input on AIN0 from the ADC but if I change the signal input to another value during runtime I notice that the new value is not read or updated it continues to show the previous value until I do a reset or re-start of the MCU. I tried looking at all my ADC settings but I don't see anything that looks incorrect. Any help or suggestions as usual will be greatly appreciated. I have attached my zipped project file.