Sorry for late reply regarding your remaining question: "The number of channels must be the same for all ADCs to operate Multi ADC? That means I can't use 1 channel of ADC2, 2 channels of ADC1 and 6 channels of ADC3?"Here is the reply from my colleag...
There was an issue in the previous STM32CubeMX v6.7.0. It shouldn't have allow SMPS with VOS0.STM32CubeMX v6.8.0 is following the device datasheet.On STM32H745, VOS0 cannot be used with SMPS.This is specified in the datasheet.See section 3.5.3 (extra...
ADCy_AWDx_OUT is an internal signal, it cannot be attached to the I/O pins.See RM0394:Each analog watchdog is associated to an internal hardware signal ADCy_AWDx_OUT(y=ADC number, x=watchdog number) which is directly connected to the ETR input(extern...
STM32L433 has 64kB SRAM composed of SRAM1 (48KB) and SRAM2 (16kB).As described in datasheet section 3.5:• 48 Kbyte mapped at address 0x2000 0000 (SRAM1) • 16 Kbyte located at address 0x1000 0000 with hardware parity check (SRAM2). This memory is al...