cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-64 7 bit serial

DOrch.1
Associate II

I am using the Nucleo-64 STM32L476 evaluation board and am connecting via the (USB) debug port. This connects to USART2. However, when I send 7 bit serial (from the PC) it appears to arrive as 8 bit serial  (USART2). Does the USB to Serial converter in the debug port only support 8 bit serial?

3 REPLIES 3

Good question, not sure

Show the configuration of ALL the uarts/serial ports in the chain here.

You're likely going to get the data as 8-bit bytes, if you've enabled parity that's included in the data-bit budget on STM32, and you'll need to strip it from the high-order bit of bytes in received data packets.

The output UART on the ST-LINK's STM32F1 should be a very close proxy of the settings you made on the PC. On the L4, it will be whatever you select there.

Why is 7-bit important? Forty years in, this seems atypical..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

@Tesla DeLorean wrote:

Good question, not sure


Indeed - it's not mentioned in the User Manual.

 


@Tesla DeLorean wrote:

Why is 7-bit important? Forty years in, this seems atypical..


+1

@DOrch.1 if it is important, maybe test with separate USB-to-UART ?

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

I am doing a quick port of some old code the STM32. The code uses an old protocol based on 7 bit serial. If I set the USART2 to 8 bit the comms work whether I set the PC to 7 bit or 8 bit. If I set the USART to 7 bit the comms don't work whether I set the PC to either 7 or 8 bit.

 This not a major issue since I am sure the final hardware will work. But this is the second limitation in the debug port that I have found. I just wanted to confirm that this was a limitation and not a mistake on my part.