2024-11-19 4:24 AM
Hello,
I am working with the STM32H7S78-DK board, and I have enabled the UART4 serial interface (using PD0/PD1) for both programming and debugging. However, I am unable to print logs to the Putty terminal.
Environment:
I have set following parameters ,
• 115200 bps
• 8-bit data
• No parity
• One-stop bit
• No flow control
Here is my code
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2024 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "stdio.h"
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
static void MX_GPIO_Init(void);
static void MX_UART4_Init(void);
/* USER CODE BEGIN PFP */
#if defined(__ICCARM__)
/* New definition from EWARM V9, compatible with EWARM8 */
int iar_fputc(int ch);
#define PUTCHAR_PROTOTYPE int iar_fputc(int ch)
#elif defined ( __CC_ARM ) || defined(__ARMCC_VERSION)
/* ARM Compiler 5/6*/
#define PUTCHAR_PROTOTYPE int fputc(int ch, FILE *f)
#elif defined(__GNUC__)
#define PUTCHAR_PROTOTYPE int __io_putchar(int ch)
#endif /* __ICCARM__ */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/* USER CODE BEGIN PFP */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Update SystemCoreClock variable according to RCC registers values. */
SystemCoreClockUpdate();
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_UART4_Init();
/* USER CODE BEGIN 2 */
/* Output a message on Hyperterminal using printf function */
printf("\n\r UART Printf Example: retarget the C library printf function to the UART\n\r");
printf("** Test Start successfully. ** \n\r");
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
printf("Hello from STM32H7S78-DK!\n\r");
HAL_Delay(1000); // 1-second delay
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief UART4 Initialization Function
* @PAram None
* @retval None
*/
static void MX_UART4_Init(void)
{
/* USER CODE BEGIN UART4_Init 0 */
/* USER CODE END UART4_Init 0 */
/* USER CODE BEGIN UART4_Init 1 */
/* USER CODE END UART4_Init 1 */
huart4.Instance = UART4;
huart4.Init.BaudRate = 115200;
huart4.Init.WordLength = UART_WORDLENGTH_8B;
huart4.Init.StopBits = UART_STOPBITS_1;
huart4.Init.Parity = UART_PARITY_NONE;
huart4.Init.Mode = UART_MODE_TX_RX;
huart4.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart4.Init.OverSampling = UART_OVERSAMPLING_16;
huart4.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart4.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart4.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart4) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetTxFifoThreshold(&huart4, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetRxFifoThreshold(&huart4, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_DisableFifoMode(&huart4) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN UART4_Init 2 */
/* USER CODE END UART4_Init 2 */
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief Retargets the C library __write function to the IAR function iar_fputc.
* @PAram file: file descriptor.
* @PAram ptr: pointer to the buffer where the data is stored.
* @PAram len: length of the data to write in bytes.
* @retval length of the written data in bytes.
*/
#if defined(__ICCARM__)
size_t __write(int file, unsigned char const *ptr, size_t len)
{
size_t idx;
unsigned char const *pdata = ptr;
for (idx = 0; idx < len; idx++)
{
iar_fputc((int)*pdata);
pdata++;
}
return len;
}
#endif /* __ICCARM__ */
/**
* @brief Retargets the C library printf function to the USART.
*/
PUTCHAR_PROTOTYPE
{
/* Place your implementation of fputc here */
/* e.g. write a character to the LPUART1 and Loop until the end of transmission */
HAL_UART_Transmit(&huart4, (uint8_t *)&ch, 1, 0xFFFF);
return ch;
}
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @PAram file: pointer to the source file name
* @PAram line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
Any guidance or troubleshooting tips would be greatly appreciated.
Thank you for your support.
Best regards,
Mehul
2024-11-19 6:07 AM - edited 2024-11-19 6:20 AM
Hello,
Did you try first sending chars by just using HAL_UART_Transmit() ?:
Example:
HAL_UART_Transmit(&huart4, (uint8_t *)"Test", 4, 0xFFFF);
You need to validate that part first before going ahead to the redirection of printf.
And what is the IDE you are using? IAR?
2024-11-19 9:26 PM
Hi thanks for answering,
I am using STM32CubeIDE (https://www.st.com/en/development-tools/stm32cubeide.html) for development.
I have tried this ,
HAL_UART_Transmit(&huart4, (uint8_t *)"Test", 4, 0xFFFF);It works as expected, but when trying to use
printf("Hello from STM32H7S78-DK\n\r");it doesn't works.
Thanks.
Best regards,
Mehul
2024-11-21 12:28 AM
Hi Mehul
printf knows nothing about &huart4 so you have to overwrite
the
#define PUTCHAR_PROTOTYPE int __io_putchar(int ch)look at
there is the how to....
HTH
padawan
2024-11-26 7:45 PM
It doesn't work but I noticed something in the .ioc file seems like UART4 is conflict with LTDC.
here i attached screenshot of .ioc file,
Best regards,
Mehul
2024-11-27 3:32 AM
These warnings are generated by CubeMX as a precaution, and you can ignore them as long as CubeMx allows you to configure the UARTs with features that you need.
The conflict here is with Asynchronous mode. Try change this mode and it will work for you.