2024-08-25 11:44 PM - last edited on 2024-08-26 8:01 AM by mƎALLEm
Hey im trying to blynk led on stm 32 l562e dk board i had attached the consol logs its not connecting to debuger i want to ask you is their any default jumper settings for this board or is their any specific debug settings required for this board . i had also attached photos of my jumper setting. additonally i had also attached my code. its a brand new board i just orderd .
STMicroelectronics ST-LINK GDB server. Version 7.8.0
Copyright (c) 2024, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Regards,
Gaurav N.
2024-09-02 5:00 AM
No i had not modified anything simple led blink project and blynk project are also not working.
2024-09-02 9:53 PM - edited 2024-09-02 9:54 PM
No i had not modified anything im using simpal blynk led code whithout any security feature or option byte you can check the code i had shaired even a blank tamplet code or sample codes from st giving same error . can also check the erros screenshots i had attached previsouly .
2024-09-09 10:23 PM