2025-11-25 1:40 AM - last edited on 2025-12-21 4:21 PM by ELABI.1
Hello,
I try to get data from a X-NUCLEO-53L8-A1 board connected to a Nucleo board and visualize it in my computer. If I use the VL53L8CX Gui and connect my COM port and click on the start button, it is working well. However, I would like to get data outside of the app (ex: Tera Term or python script) but I do not have data available. I suppose that the sensor/board is waiting for "start" but I can not find any documentation on the subject.
Can someone help me on the subject ?
Best regards
2025-11-25 5:55 AM
Hello @thogat ,
Are you using latest version of X-CUBE-TOF1 ?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-11-25 6:03 AM
Hello @FBL ,
I tried to use the lastest version but I could not get any connection options on VL53L8CX_GUI as I could not see any COM port. So I used the button "Flash FW" and I manage to connect the board and get data on the app. On the other hand, I tried to connect to the COM port using Tera Term but no data were available.
Then, I flashed the lastest version of X-CUBE-TOF1 and I got the message :
"VL53L8A1_RANGING_SENSOR_In it failed Check you're using ONLY the center device soldered on the shield, NO satellite shall be connected !"
2025-12-15 12:41 AM
Hi
The GUI code doesn't support the human readable format output, I attached an PSN code for interact between laptop and X-NUCLEO-53L8-A1 through USART interface,
Br
Zhiyuan.Han