cancel
Showing results for 
Search instead for 
Did you mean: 

no target found

suhfi
Senior

I am using nucleo-144, H743ZI2 board. while i am uploading code in the stm32cubeide i am getting error as "target not found". i have searched in the community and then tried connect the boot0 to high, and power the board, connect to cube programmer and erase full chip flash memory. while i do that i am not able to connect board. i am getting an error as: no stm32 target found. i have tried to connect boot 0 to vcc and power it. In the cube programmer i am unable to get the connect. and i have gone through the user manual of the board h743zi2 board, but there also i received the same answer. when i connect or power the board, we get the firmware right, i am getting mbed, details and failed document also. In the fail text document i have "The interface firmware FAILED to reset/halt the target MCU". what should i do? I want to upload the new code and will it be possible to erase the old code. I have checked the vdd(JP4). i got around 2.5 volts which might be near to 3.3volts and while uploading the code, i am getting the same problem as stm32 target not found. and in cube programmer also i am unable to connect it. is this board working. how can i troubleshoot it?

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello @suhfi 

Why are you still duplicating the same subject?

https://community.st.com/t5/moderation-archive/target-not-found-stm32h743zi2/td-p/718012

https://community.st.com/t5/stm32-mcus-products/target-not-found-error-in-stm32h743zi2/td-p/716168

2.5 volts is not the correct voltage as you are supplying the board over ST-Link. need to have either 1.8V or 3.3V.

If you have another board please check that. Otherwise you can purchase another one as I suspect you have a regulator issue on the board.

And again, please don't duplicate this subject again.

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

1 REPLY 1
SofLit
ST Employee

Hello @suhfi 

Why are you still duplicating the same subject?

https://community.st.com/t5/moderation-archive/target-not-found-stm32h743zi2/td-p/718012

https://community.st.com/t5/stm32-mcus-products/target-not-found-error-in-stm32h743zi2/td-p/716168

2.5 volts is not the correct voltage as you are supplying the board over ST-Link. need to have either 1.8V or 3.3V.

If you have another board please check that. Otherwise you can purchase another one as I suspect you have a regulator issue on the board.

And again, please don't duplicate this subject again.

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.