2011-03-23 12:14 AM
Hello,
I'm totally novice and need your help. I have installed the lastest version of the MDK-ARM from keil. The result of the compilation is good, but when try to download the programm to the uC, the Software launch one message: ''NO ST-Link Detected
''. When I connect the DISCOVERY board to my USB, the led Blinks correctly, andand
I
could
update
the
firmware
of
the
system without
problems
.
Where is my problem? Thanks!2011-03-23 12:56 AM
Seems to work fine with 4.12 on Windows XP, and Vista 32-bit. STLink\ST-LINKIII-KEIL.DLL V1.5.1
What version, and OS are you using? Make sure you have selected SWD mode in the configuration pane. That the \Keil\ARM\STLink directory contains the latest driver files. Check that the current user has Admin rights. Do the ST-LINK utilities works? Is that app closed?2011-03-23 04:59 AM
Thanks for your reply clive1,
I have MDK-ARM 4.12 and WinXP.
Yes, I selected SWD in the ST-Link Setup. My directory file C:\Keil\ARM\STLink contain: - ST-LINKIII-KEIL.dll - STLinkUSBDriver.dll - stm32f10xGLoader.bin - stm32f10xLoader.bin - stm32wLoader.binI will try if the ST-LINK utilities works, but seems that the Discovery board connect successfull whit the PC because I updated successfull the firmware of the ST-link with the ST-LinkUpgrade.exe
Regards!
2011-03-23 02:03 PM
Hello,
with the STM32 ST-LINK Utility also don't work. Where is my problem? The problem is the WinXP? The St Drivers? ... Thanks!2011-03-23 11:37 PM
with the STM32 ST-LINK Utility also don't work. Where is my problem?
Dunno, perhaps your ST-LINK is busted, try it on a different PC. If this is a VL discovery, do you still see the ''flash drive'' instantiation with the webpage/links to the documentation files when you plug it in. Does your account have administrative rights? Do you have some AV software that might interfere with normal operations?2011-03-24 04:50 AM
2011-03-25 05:16 AM
What is the VL Discovery?
Honestly? You are posting on the STM32VL-Discovery forum. I was just try in make sure we were talking about the same thing, because the ST-LINK was available as a stand-alone JTAG pod look before it was integrated onto other boards. Did it work properly before you updated the firmware, the devices I got from the first production run worked fine without one. Do you have any additional boards you could try, or did you jut get one?2011-03-25 06:16 AM
Thanks for your support clive1,
finally this morning I have ordered to EBV (Avnet) one pair more of STM23VLDiscovery boards, and one ST-Link. I never got a good communication with the PC, which this reason I upgrade the firmware on the board.
2011-03-25 08:37 AM
Perhaps you just got a dud. I picked up a handful for assorted projects and developers, they all seem to work fine across a range of PC's using XP and Vista.
2011-03-29 10:45 PM
Bad News, after test with 3 STM32VLDISCOVERY and one ST-LINK in 3 differents PC's, the result is the same: ''NO STLINK Detected''. Now, I think that the problem maybe the Windows XP in Spanish. I will try to test in one PC with XP in english.