2024-05-08 2:07 AM - edited 2024-05-08 2:11 AM
I am using a Nucleo F401RE board to drive a PCM5102a PCM Audio Codec via I2S.
My goal is to send data from a double buffer via DMA.
Since I am only using the Audio Codec as an output, I configured my I2S as Half-Duplex Master in CubeMX.
Now to my problem:
In the generated I2S HAL driver stm32f4xx_hal_i2s_ex.c, there is no DMA Callback registered for Transmit Cplt or HalfCplt:
I am calling HAL_I2SEx_TransmitReceive_DMA in main.c, to start the DMA cycle. everything works fine, except Callback invocation. Here is the corresponding snippet in the generated HAL_I2SEx_TransmitReceive_DMA, that prevents Tx Callbacks.
/* Set the I2S Rx DMA Half transfer complete callback */ hi2s->hdmarx->XferHalfCpltCallback = I2SEx_TxRxDMAHalfCplt; /* Set the I2S Rx DMA transfer complete callback */ hi2s->hdmarx->XferCpltCallback = I2SEx_TxRxDMACplt; /* Set the I2S Rx DMA error callback */ hi2s->hdmarx->XferErrorCallback = I2SEx_TxRxDMAError; /* Set the I2S Tx DMA Half transfer complete callback as NULL */ hi2s->hdmatx->XferHalfCpltCallback = NULL; /* Set the I2S Tx DMA transfer complete callback as NULL */ hi2s->hdmatx->XferCpltCallback = NULL;
This of course makes sense when using DMA RxTx at the same time so that the Callbacks only trigger once per RxTx/RxTxHalf. But since I set I2S to Transmit only (Half-Duplex), the callbacks won't fire at all.
Is this expected behavior?
Best, jonas
Solved! Go to Solution.
2024-05-08 2:19 AM
(I have used the F401 to play audio - working fine, as long as using standard I2S with 16bit data.)
How you set the chip ? with Cube/HAL ? (I did ; works as expected.)
To get the callbacks (+ yes, only for Tx , with circular DMA ) set in Cube : Callback enable I2S ...see:
2024-05-08 2:19 AM
(I have used the F401 to play audio - working fine, as long as using standard I2S with 16bit data.)
How you set the chip ? with Cube/HAL ? (I did ; works as expected.)
To get the callbacks (+ yes, only for Tx , with circular DMA ) set in Cube : Callback enable I2S ...see:
2024-05-08 3:01 AM
Thanks a lot, i forgot to register the i2s Callbacks. Since the DMA Callbacks are automatically registered for RxTx, i would't think of registering i2s Callbacks seperately.