2015-01-14 8:48 AM
New release of Raisonance tools for STM32 is now available with support of new MCU variants in STM32 L4, F3, F4 and F7 lines.
This software supports both the RLink and ST-Link debugger/programmers.The support Raisonance support web site address has changed to support.raisonance.com
You can download the latest software using the following links:RKit-ARM (GCC compiler chain)
:2015-07-16 6:58 AM
Note, there is also a special offer for unlimited versions with no debug limitation. This offer will run until end of September 2015. More info at: