STM32F407 User Button not working after setting up Clock and Bus Frequency
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-06-26 10:57 AM
Good Evening all,
I am new to Embedded Programming. I am using STM32f407vgt6 discovery board for programming. I am using HAL functions for setting up the SYSCLK and BUS frequencies. In this program , after one presses USER button , LED should blink. LED is blinking normally in case I don't use HAL libraries. But after I have set the clock speed using HAL libraries , the user button does not work. Could someone please help me in finding why the user button PA0 does not function ? Here is my code (I am using CooCox IDE) : //&sharpinclude ''stm32f4xx.h'' //&sharpinclude ''stm32f407xx.h'' &sharpinclude ''stm32f4xx_hal.h'' &sharpdefine GPIO_TogglePE8() (GPIOE->ODR ^= (uint16_t)0x0100) /* Pin 8 selected */ uint32_t sysclockfreq1; uint32_t HCLK11; uint32_t PCLK11; uint32_t PCLK21; TIM_HandleTypeDef htim5; void SystemClock_Config(void); int main(void) { /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* Configure the system clock */ SystemClock_Config(); // Debug Purpose sysclockfreq1=HAL_RCC_GetSysClockFreq(); HCLK11=HAL_RCC_GetHCLKFreq(); PCLK11=HAL_RCC_GetPCLK1Freq(); PCLK21=HAL_RCC_GetPCLK2Freq(); RCC->AHB1ENR |= 0x0019; // Enable clock for GPIOE & GPIOD & GPIOA RCC->APB1ENR |= 0x00000008; // Enable Clock for Timer 5 GPIOE->MODER |= 0x00010000; // Output pin for time mark at port E bit 8 GPIOD->MODER |= 0x04000000; // Output pin for PD13 LD3 Orange GPIOA->MODER |= 0x00000000; // Input pin for reading User Button PA0 while(!(GPIOA->IDR & 0x01)); //wait when PA0=0 GPIOD->ODR |= 0x2000;// The program control does not reach this line even after pressing the user button ( But during debugging the control is coming here) HAL_NVIC_EnableIRQ(TIM5_IRQn); // Enable IRQ for TIM5 in NVIC. TIM5_IRQn present in stm32f407xx.h TIM5->ARR = 8400; // Auto Reload Register value => 0.1 ms TIM5->PSC = 9; // => 1 ms TIM5->DIER |= 0x0001; // DMA/IRQ Enable Register - enable IRQ on update TIM5->CR1 |= 0x0001; // Enable Counting HAL_TIM_IRQHandler(&htim5); while(1) { //GPIOD->ODR |= 0x2000; } } void SystemClock_Config(void) { // Enabling the external crystal Clock // Enable HSE Oscillator and Activate PLL with HSE as source RCC_OscInitTypeDef RCC_OscInitStruct; RCC_ClkInitTypeDef RCC_ClkInitStruct; //__PWR_CLK_ENABLE(); //This is to enable access to the RTC Domain and RTC registers //__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1); RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 8; RCC_OscInitStruct.PLL.PLLN = 336; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = 4; HAL_RCC_OscConfig(&RCC_OscInitStruct); if (HAL_RCC_OscConfig(&RCC_OscInitStruct)== HAL_OK) { // do printf. Could also turn on LED to indicate that HSE isn't running well RCC->AHB1ENR = 0x0000008; // Enable Clock for PortD GPIOD->MODER |= (1<<30); // Enable PortD Pin 15 as a digital output GPIOD->ODR |= (1<<15); // Turn GPIO Pin 15 ON or Assert High } // Select PLL as system clock source and configure the HCLK, PCLK1 // Clocks dividers RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1 |RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2; HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5); if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5)== HAL_OK) { // do printf. RCC->AHB1ENR = 0x0000008; // Enable Clock for PortD GPIOD->MODER |= (1<<28); // Enable PortD Pin 14 as a digital output GPIOD->ODR |= (1<<14); // Turn GPIO Pin 14 ON or Assert High } } #stm32- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-06-30 4:45 AM
Hello,
I recommend you to use either Standard peripheral Library or HAL library, avoid to merge code of each of them. After that, maybe the problem will be solved. Regards- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-06-30 7:45 AM
I recommend you to use either Standard peripheral Library or HAL library, avoid to merge code of each of them. After that, maybe the problem will be solved.
The OP stated he was using HAL, and I see no SPL code there. There's some register level stuff, which is perhaps beyond the experience shown. I agree mixing coding methods would seem to be a poor choice.
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
‎2015-07-16 6:41 AM
Thank you so much for your response. I now used SPL instead of HAL to set up the clock frequency. I still did the programming at register level and got no errors.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-07-16 7:20 AM
The compiler saying there are ''no errors'', means there are no egregious syntax errors, not that the code is functionally correct.
Up vote any posts that you find helpful, it shows what's working..