cancel
Showing results for 
Search instead for 
Did you mean: 

My adc is measuring -3,3 to 3,3 that 16 bit but I wanna build it as 0 3,3 V how can I configure it in this form?

situ.1
Associate II
 
1 ACCEPTED SOLUTION

Accepted Solutions

None of the STM32 support ADC of +/- 3.3V

Perhaps you be more specific, and detail how this is relevant to the forum

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

7 REPLIES 7

None of the STM32 support ADC of +/- 3.3V

Perhaps you be more specific, and detail how this is relevant to the forum

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
situ.1
Associate II

STM32H743 I have connected PC with usb cable supplyin power from it.

When I apply 0 V I read 32768 approx.

Then I appiled -3.3 volt the it comes 0 Volt.

I wanna use it as 0 3.3 V and 16 bit please help!

LauraCx
ST Employee

Modified by moderation.

We kindly remind you to keep a friendly tone when writing your questions, Community is about people helping each other. :)

What board is this? A custom one? Share a circuit diagram, illustrate what you're trying to do.

The IC is not designed to take -3.3V on any of the input pins

I'd imagine doing so would probably cause damage to the IC or the pin in question.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
situ.1
Associate II

STM32H743ZIT6 . I am trying to measure 0 3.3 V from ADC and make it as 16 bit.

When I connect jumpers to pins that shows in photo and When I apply 0 V I read 32768 approx...

I wanna get this measurement between 0 and 3.3 Volt. Thankss

0693W00000SuO5sQAF.png

situ.1
Associate II

And when I connect this pins -3.3 Volt I got 0 Value as digital thats proof of it works -3.3 +3.3 for 16 bits

STM32H743ZIT6 is a CHIP, not a BOARD

What BOARD is this on, and what's the CIRCUIT?

Why are you connecting -3.3V, this is way outside the absolute maximums? Damagingly

so.

Make sure you have a common ground between the STM32 and whatever else you're connecting too.

Make sure VSSA is this same Ground, and VDDA is 3.3V

DON'T go above/below this limits

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..