cancel
Showing results for 
Search instead for 
Did you mean: 

MSI with LSE auto calibration accuracy

Steffen Rose
Associate III

Has the MSI with LSE auto calibration a sufficient precision for the 1Mbit CAN bitrate?

What is the accuracy compared with a crystal PLL clock?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User

ST states that MSI with LSE autocalibration is good as a FS USB clock. USB standard requires FS signaling to have timing error less than 0.25%. Is this sufficient for 1Mbit CAN bitrate?

JW

Example calculations say 0.5% for 1Mbit/s, but it's depend of the specific environment.

Thank you.