cancel
Showing results for 
Search instead for 
Did you mean: 

Moving from AVR to STM32 -- starter questions

artvolk
Associate II
Posted on January 05, 2011 at 12:18

Moving from AVR to STM32 -- starter questions

18 REPLIES 18
artvolk
Associate II
Posted on May 17, 2011 at 14:20

About EEPROM, it seems I've found app note:

AN2594 EEPROM emulation in STM32F10x microcontrollers

Andrew Neil
Evangelist III
Posted on May 17, 2011 at 14:20

About EEPROM emulation, see:

[DEAD LINK /public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/ARM CortexM3 STM32/hi,&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E]https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fARM%20CortexM3%20STM32%2fhi%2c&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E

artvolk
Associate II
Posted on May 17, 2011 at 14:20

Thanks for the response! What about other items, what IDE\compiler do you use?

baranovus
Associate III
Posted on May 17, 2011 at 14:20

I bought ST-LINK at DigiKey and it didn't work at all. Just lost my money.

kurtkraus2
Associate
Posted on May 17, 2011 at 14:20

- IAR  maybe the most used for arm and defacto the standard for ARM CPU's

- KEIL close the same as IAR. A lot of samples and Eval Boards working with Keil and IAR

IAR has the very good Powerpac Lib. Keil has also a nice Libraries.

BTW. You will need a JTAG Programmer Ulink oder IAR-Link. RS232 Serial programming is a pain in the...

There a lot of others in the Market. Maybe download the ST Fimware examples and you will find for programmed examples for those compliers

Have fun. 0x0000000000000001

Posted on May 17, 2011 at 14:20

Thanks for the response! What about other items, what IDE\compiler do you use?

It's probably not GCC, and your original question seems to be artificially constrained.

I think RIDE, ROWLEY and ATOLLIC use GCC, but it's hardly what I'd call an ''embedded'' compiler. Of those I would choose Rowley, or just use WinARM or Yagarto.

I'm also not sure what ''community choice'' is. Is it code for free or cheap, or runs under Linux? Development environment choice is typically personal (what you like/prefer), or corporately driven (what the vendor/customer uses). The aggregated opinion of the forum is unlikely to result in a single clear answer, everyone will have their own preference, usually a strong one.

The Keil or IAR demo/eval versions would be my suggestions. Atollic Lite is so broken/crippled/slow as to be unusable, and the buy-in prices for the TrueStudio could get you equivalent Keil tools with a lot more mileage.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on May 17, 2011 at 14:20

BTW. You will need a JTAG Programmer Ulink oder IAR-Link. RS232 Serial programming is a pain in the...

He's using a VL Discovery board, with the built in ST-LINK.

Notwithstanding that programming with the serial port is *not* that hard and readily implemented on a production line, for debugging you do indeed need a decent JTAG or trace tool.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Evangelist III
Posted on May 17, 2011 at 14:20

''I can't speak to it's effectiveness for debugging''

 

I use Keil, but it seems to me that by far the biggest problem with all of the free GCC-based things is getting debug working!

With Keil (and IAR), you get a complete kit that ''just works''; with the free GCC-based things, you get the compiler from here, the debugger from there, a patch from somewhere else, pull together a few forum threads to configure it, etc, etc, etc,...

Well, that's the way it looks to me, anyhow!
artvolk
Associate II
Posted on May 17, 2011 at 14:20

Thank you for the responses, you are absolutely correct about ''It's probably not GCC, and your original question seems to be artificially constrained'', I just have last hope that something like WinAVR exists for STM32. It seems IAR is the way to go for me (at least it seems to be the most popular).

Some other questions left:

- Will ST-Link part of STM32VL-Discovery work with other STM32 controllers, for example F103 line?

I assume the answer is ''yes''?