2011-01-05 03:18 AM
Moving from AVR to STM32 -- starter questions
2011-05-17 05:20 AM
Pull a couple of jumpers, and hook up a couple of wires would suffice for the SWD interface. Bit kludgy for my tastes, but $10 is pretty cheap for the JTAG/SWD function. ST lists the supported CPU models on their website somewhere.
I think the WinARM and WinAVR both use GCC compilers, WinARM is certainly capable of generating viable STM32 code. I can't speak to it's effectiveness for debugging. http://winarm.scienceprog.com/winarm-tools/what-are-differences-between-winarm-and-winavr.html2011-05-17 05:20 AM
Thank you all for the responses!
I do want simple debugging support out of the box, that's one of the reasons I've ordered ST32VL-Discovery (haven't got it yet, though). As far as I can tell from these and other forums, I have two possibilities to get OnChip debug support: - Use STM32 Discovery with IAR or Keil (limited free versions or commercial) - Use CoLinkEx (free, but works at least with F103 line) Have I missed any options?2011-05-17 05:20 AM
''I do want simple debugging support out of the box''
I can confirm that the free Keil Evaluation download will do this. I would very much suspect that IAR will, too (but haven't tried it).2011-05-17 05:20 AM
Wrong piece? Nowadays Keil, IAR and others support ST-Link as a debug tool, too, and they have libraries for it integrated!
2011-05-17 05:20 AM
Thank you for the quick and accurate responses! Can't wait when my STM32VL-Discovery arrive 🙂
2011-05-17 05:20 AM
i`m using usbscarab and oocdlink debuggers, both with usb + codesourcery + openocd + eclipse + zylin.
there is huge tutorial but unfortunatelly in polish, but you can translate it with google: http://www.freddiechopin.info/index.php/pl/artykuly/35-arm/59-arm-toolchain-tutorial those debuggers are very cheap, below 20$, the rest are free to download and use from internet.2011-05-17 05:20 AM
''i`m using usbscarab and oocdlink debuggers, both with usb + codesourcery + openocd + eclipse + zylin''
That's a whole lot of stuff that you've had to obtain, configure, and integrate! And that is my point: when you get Keil or IAR (probably others), you get a complete package; with ''free'' (sic) open source, it seems to me, you have to put (a great deal of) effort into obtaining and assembling a ''system'' With the paid-for open-source offerings, it seems to me that the thing you pay for is having the supplier do all this work for you... Again, this is just the impression of one having looked at it, but not actually done it.''there is huge tutorial'' It is just ''huge'' because it's so complicated...?😉2011-05-17 05:20 AM
Not excactly a Linux port of ST-Link
How about Versaloon ported to run on the JTAG part of the STM8S or the STM32VL. I just ported versaloon (SWD only) to the above board , and now i can program my STM32VL - value-line chip , on Ubuntu 10.04. Using just the STM32VL USB cable & versaloon vsprog or OOCD See http://www.versaloon.com/bbs/viewtopic.php?f=2&t=17&start=0 /Bingo2011-05-17 05:20 AM
Hey,
What happened? I also started using it, and works well for me.. Cheers, Sam